Garmin LIDAR-Lite v4 (Qwiic) Hookup Guide

≡ Pages
Contributors: santaimpersonator, MAKIN-STUFF

Resources and Going Further

Looking for other distance sensors? Check out some of these tutorials:

Qwiic Distance Sensor (RFD77402) Hookup Guide

The RFD77402 uses an infrared VCSEL (Vertical Cavity Surface Emitting Laser) TOF (Time of Flight) module capable of millimeter precision distance readings up to 2 meters. It’s also part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out how far away things are.

Qwiic Distance Sensor (VL53L1X, VL53L4CD) Hookup Guide

The Qwiic Distance Sensor - VL53L1X is a time of flight sensor that is capable of several modes, as well as having a range of 4M. It's cousin VL53L4CD is also a time of flight sensor with similar characteristics but it has a range of about 1.3M. Let's hook it up and find out just how far away that thing over there is.

Getting Started with the A111 Pulsed Radar Sensor

Get started with the Acconeer A111 SDK with a Raspberry Pi! The tiny A111 pulsed coherent radar (PCR) adds high-precision, cutting-edge distance measurement for speed-, material-, motion-, or gesture-sensing projects! We’re not talking about simple ultrasonic, or even infrared sensors here, but 60GHz radar!

Qwiic Ultrasonic Distance Sensor (HC-SR04) Hookup Guide

Get started with the Qwiic Ultrasonic Distance Sensor!