Firefly Jar Assembly Guide

≡ Pages
Contributors: b_e_n, Mando

Step 10: Cover it Up

NOTE!

This felt pattern is now FLIPPED OVER TO THE FRONT FACING SIDE.

alt text

  1. Make sure to leave the back side of the sewn felt exposed so you can access the battery holder and switch.

There are two ways you can finish your firefly jar:

A. Lay the unused felt you set aside earlier over the LED exposed side of the sewn felt. Sew the edges together with regular thread or

B. Spray glue the unused felt. Stick that piece to the LED exposed side of the sewn felt.