ESP32 Thing Motion Shield Hookup Guide

≡ Pages
Contributors: MTaylor

Hardware Overview

The hardware is a conglomeration of an SD card socket, LSM9DS1 IMU, and GPS serial port. There's also an LED for general indication.

Motion Shield Parts

All components are populated on the top of the board. Here, you can see the SD card, IMU, and port. The ESP32 Thing is intended to sit above this board, so no pins are labeled.

Back of Motion Shield

There are no options on the bottom side. Here, you'll find labels for all of the pins. The two rows of pins on the side are wired together so that you have one available for prototyping after installing an ESP32 Thing.

The signals that are used are show here, grouped by function.

ESP32 Thing Pin Direction Signal Group ESP32 Function
GPIO 13 I LED LED GPIO 13
GPIO 16 I GPS_TX GPS UART Serial 1
GPIO 17 O GPS_RX GPS UART Serial 1
GPIO 18 I SD_SCK SD Card SPI SCK
GPIO 19 O SD_DO SD Card SPI MISO
GPIO 23 I SD_DI SD Card SPI MOSI
GPIO 33 I
SD_CS SD Card GPIO 33
GPIO 38 I
SD_CD SD Card GPIO 38
GPIO 21 I/O SDA IMU I2C SDA
GPIO 22 I SCL IMU I2C SCL