Displaying Sensor Data with Bluetooth
Contributors:
lauren gregory
Resources and Going Further
Given a few modifications to the code, this project can be adjusted to accommodate a wide variety of sensors. Instead of the KX132 Triple Axis Accelerometer, try sending data from STTS22H Temperature Sensor or the SGP40 Air Quality Sensor! Collecting and storing data over a longer period of time could also be a useful extension of this project
The following tutorials may also be useful:
I2C
An introduction to I2C, one of the main embedded communications protocols in use today.
Bluetooth Basics
An overview of the Bluetooth wireless technology.
Triple Axis Accelerometer Breakout - KX13x (Qwiic) Hookup Guide
Get started measuring acceleration and vibration using the Triple Axis Accelerometer Breakout - KX134 (Qwiic) & KX132 (Qwiic) following this Hookup Guide.
ESP32 Thing Plus (USB-C) Hookup Guide
Meet the updated ESP32 Thing Plus (USB-C) development board. We have included some extra bells and whistles that users will appreciate, so check out out hookup guide for all the details!