Connectivity of the Internet of Things

≡ Pages
Contributors: RBERLIA

ZigBee

alt text

Source: Zigbee.org

Zigbee, like thread is an alliance of over 200 companies which have collaborated to develop a robust and simple network for home and industrial automation.

Zigbee Design Goals

Zigbee was created for the sole purpose of serving the home and industrial automation, so the design goals are set in accordance to that:

  • Low-power
  • Security
  • Co-existence with other radio networks which use the ISM band.
  • Standardization
  • Low-cost

Similar to Thread, ZigBee is built on top of the IEEE 802.15.4 standard.

ZigbEE specifications fills in the gap left by the 802.15.4 to create a true mesh network but also supports other topologies like Star and Tree.

alt text

Source - AMX - Zigbee White Paper

Devices in a Zigbee Network

There are three types of devices as defined by the Zigbee protocol:

  • Zigbee Coordinator
  • Zigbee Router
  • Zigbee End Device (Node)

Zigbee Coordinator

The coordinator is the brains of the Zigbee network, it commissions devices to the network, stores the security keys and also bridges to other networks. There is only one Zigbee Coordinator in any network.

Zigbee Router

Zigbee Networks may have several routers to serve as intermediate routers or to transmit data within the network.

Zigbee End Device

The end device can only talk to the parent node ( router or coordinator). It cannot talk to other end devices directly. Similar to Thread, these devices are designed by keeping in mind that they spend most of their life times in sleep mode and only wake up to transmit data to the parent.

ZigBee assumes the channels from 11-26 in the 2.4GHz radio band used by most radios. The ZigBee channels have been specifically spaced as to co-exist with Wi-Fi channels without interference, if the channel assignments of both the networks are properly.

alt text

Source - eetimes.com

Note: The best spectral usage for both is achieved by setting the Wi-Fi channels to 1, 6, 11 and Zigbee channels to 15, 20, 25.

Zigbee vs Thread

ZigBee standard faced a big challenge when Thread came into existence in 2014. The ZigBee Alliance has then pushed to introduce their newest protocol called the ZigBee 3.0. They have tried to address the areas, where thread and other networks were better alternatives in the home automation space.

alt text

ZigBee 3.0 came with additional features such as ZigBee RF4CE and ZigBee Green Power.

ZigBee RF4CE - was developed to replace the IR remote with radio based remotes. This is aimed at making an universal remote controller that could be used to control your remote and as well as lights, lamps etc. Also this does away with the point and shoot limitation of IR.

ZigBee Green Power - was developed as an ultra-low power standard to support energy harvesting devices. It ensures very low power consumption by managing the network as such that these devices can be off for the most time.

One major feature that put ZigBee behind thread was IP compatibility. ZigBee 3.0 on the other hand is fully IP compatible. So you can now connect your ZigBee devices to the internet via a router.

Advantages: Pretty much the same as thread

Disadvantages: Short range, Low data speeds

Xbee's by Digi International are radio communication modules which support the Zigbee Protocol. They can also be loaded with firmwares to support Zigbee Pro and DigiMesh.

To get a quick taste of Xbee, you can check out the following tutorials.

XBee Shield Hookup Guide

How to get started with an XBee Shield and Explorer. Create a remote-control Arduino!

Exploring XBees and XCTU

How to set up an XBee using your computer, the X-CTU software, and an XBee Explorer interface board.

Teensy XBee Adapter Hookup Guide

Getting started with the Teensy 3.1 / Teensy 3.2 and XBee. Establishing a serial link.