Connectivity of the Internet of Things

≡ Pages
Contributors: RBERLIA

RFID and NFC

RFID

Radio-Frequency Identification (RFID) is a communication method used for tracking and identifying objects wirelessly.

As complicated as it may seem, it is one of the simplest communication methods, which is what makes it ubiquitous and yet invisible. It is used not only in tracking consumer products worldwide, but also in tracking vehicles for toll collection. Hospitals use it to track their patients, and farmers to track their cattle. RFID technology has become a part of our lives, and we might not even be aware of how it affects us.

Simply put, we can think of RFID tags as a close replacement to Universal Product Code or the bar code. But they are more efficient.

The RFID tags have read and write capabilities over traditional bar codes. They can be updated, changed and locked.

RFID technology includes tags and readers.

Tags

The tags are the end points in an RFID system. They store identity information along with other information as required by the purpose of the tag. There are two types of tags:

  • Active Tags: These tags have an on-board power source of some sort, usually a battery, which means they can transmit stronger signals and therefore have more range. This type of tag can periodically transmit a signal irrespective of a reader.

  • Passive Tags: These tags do not have any internal power source and get activated in the vicinity of a reader. Your metro or bus pass is generally a passive tag, which gets activated when you touch it to the reader. These tags harvest the radio energy transmitted by the reader.

** Inside of an active RFID tag -- note the on-board battery**

alt text

A passive tag -- note the small size of the tag in comparison

alt text

Source: http://www.harlandsimon.co.uk

Passive RFID tags primarily operate at three frequency ranges:

* Low Frequency (LF) 125 to 134 kHz
* High Frequency (HF) 13.56 MHz
* Ultra High Frequency (UHF) 856 MHz to 960 MHz

Readers

Readers have a similar construction to an RFID tag. They have an antenna to receive and transmit signals to/from the tags. They might be either battery powered or plugged in to a wall outlet, as a reader requires strong RF signals to activate the tag (for passive) when it comes in the vicinity of the reader. The reader is connected to a reader controller, which manages the information read by the reader. The reader may also write or update a tag depending on the application. For example, the reader in subway stations is at the entry point. When the rider places a card (tag) on the reader, it reads the available money in the card and grants the user entry. At the passenger's exit, it calculates the fare and updates the amount on the card.

RFID tags can have three main components:

  • An Integrated Circuit (IC) for storing identity information, processing it and modulating/demodulating the RF signals
  • An antenna to receive and send the radio signals
  • A power source (battery) if an active tag

The reader, along with the tags, form an RFID system.

Basic RFID System

alt text

Source: www.impinj.com

The image above shows a very basic RFID system. The tag chip is the Integrated Circuit in the RFID Tag. This IC delivers computation, memory and extended features to the tag. The tag chip has an antenna to receive or transmit the information of the tagged item. The receiver's antenna receives the RF signal and might also provide excitation to a passive RFID tag. The read information is fed to a reader control and management software.

NFC

alt text

Source: techradar.com

Near-Field Communication (NFC) is an RF-based communication protocol. It is a subset of the RFID protocol, which is why it is similar to RFID but has significant differences. NFC has also become a very popular technology, and 9 out of 10 smartphones today are shipped with NFC capabilities. This has enabled contact-less payments such as Apple Pay and Google Wallet.

NFC smartphones pass along information from one smartphone to the other by tapping the two devices together, which turns sharing data such as contact info or photographs into a simple task. Applications like Android Beam facilitate this, whereas in Apple phones NFC can only be used for Apple Pay as of now.

NFC is being used to open car doors in NFC-enabled car keys with car manufacturers such as BMW. You might have also come across advertisements and marketing content that requires you to tap or wave your NFC-enabled smartphone to download an application or get more information about a product.

NFC is designed for very short-range communication (a few centimeters). It is one of the most power-efficient communication protocols. NFC also operates in the 13.56 MHz band, which is used by high-frequency RFID as well. Therefore, NFC can also read HF RFID tags.

NFC has two types of devices (one thing to note is that, in NFC, the device can act as a tag or a reader):

  • Initiator: The device that initiates the communication is labeled as the initiator. It actively generates an RF field that can power the passive target.
  • Target: This is the device that receives the information from the initiator. The target can either be passive (in the case of simple NFC tags) or active for peer to peer communication, such as in smartphones.

RFID vs. NFC

Due to the inherent similarity between these two communication protocols, we often find ourselves asking the differences in the technologies.

RFIDvsNFC

Source: RFIDinsider

Since both NFC and RFID are omnipresent technologies, used with a large set of objects and devices around us, they both are useful protocols when it comes to IoT. These protocols provide a bridge to various objects around us by not just communicating within the tag and the reader but connecting all of them to the internet.

Here are links to a few tutorials and blog posts you might want to review to learn more:


SparkFun RFID Starter Kit Hookup Guide

Learn the basics of how to get started with the SparkFun RFID Starter Kit.