Assembly Guide for RedBot with Shadow Chassis

≡ Pages
Contributors: HelloTechie, SFUptownMaker, Shawn Hymel

8. Buzzer (SIK)

Read on if you have the SIK for RedBot or are using the RedBot Buzzer. If not, skip to the next section.

Every robot should be able to make some sounds. Adding the buzzer will allow you to give your RedBot a little personality with its own beeps and bops. Adding the RedBot Buzzer is nice and easy!

Locate the Following:

1x Buzzer Board (S)
RedBot Buzzer

Add the RedBot Buzzer

Locate the SERVO port with "9" marked on the RedBot Mainboard. With the buzzer and female header side of the Buzzer Board (S) facing to the left, place the Buzzer Board on top of the "9", "POW", and "GND" male header pins.

Adding the buzzer to the RedBot