ARGOS ARTIC R2 Satellite Transceiver Shield Hookup Guide

≡ Pages
Contributors: PaulZC

Breakout Pins

The table below describes the function of each of the ARGOS ARTIC R2 Satellite Transceiver Shield breakout pins:

Pictured are the ARTIC R2 Shield breakout pins

Pin NameFunctionDescriptionNotes
CIPOOutputSPI interface: Controller In Peripheral Out.Logic level is 3.3V.
COPIInputSPI interface: Controller Out Peripheral In.Logic level is 3.3V.
SCLKInputSPI interface clock signal.Logic level is 3.3V. Typically 1MHz. See the ARTIC R2 datasheet for the permitted clock speeds.
CSInputSPI interface chip select.Logic level is 3.3V.
GNDPower ground / 0V.
G8InputGain control.Logic level is 3.3V. Pull high to set the RFPA0133 transmit power to maximum. The transmit power will be reduced by approximately 5dB if this pin is pulled low or left open.
BOOTInputConnected to the ARTIC R2 BOOT pin.Logic level is 3.3V. Pulled high via a 100k resistor. When high, the ARTIC boots from the on-board flash memory. Pull low if the ARTIC firmware will be downloaded by the MCU via SPI.
INT1OutputConnected to the ARTIC INT1 pin.Logic level is 3.3V. Will be pulled high by the ARTIC to indicate (e.g.) an RX_VALID_MESSAGE.
INT2OutputConnected to the ARTIC INT2 pin.Logic level is 3.3V. Will be pulled high by the ARTIC to indicate (e.g.) an RX_BUFFER_OVERFLOW.
RESETBInputConnected to the ARTIC reset pin.Logic level is 3.3V. Pulled high via a 100k resistor. Pull low to reset the ARTIC.
PWR ENInputShield power circuit enable.Logic level is 3.3V. Pulled low via a 100k resistor. Pull high to enable power for the ARTIC R2.
RF ENInputRF Amplifier enable.Logic level is 3.3V. Pulled low via a 100k resistor. Pull high to enable power for the RF amplifier.
VUSBPowerPower input from (e.g.) USB.Typically 5V. 6.5V maximum.
VBATTPowerPower input from (e.g.) a LiPo battery.Typically 3.6V - 4.2V. 6.5V maximum.

Power can be provided via the VBATT pin or the VUSB pin, or both. The shield will preferentially draw power from USB if connected. On-board 3.3V and 1.8V regulators regulate USB or battery power for the ARTIC R2 and RF amplifier. See below for the typical VBATT current draw.