2D Barcode Scanner Breakout Hookup Guide

≡ Pages
Contributors: El Duderino, MAKIN-STUFF

Introduction

Note on 2D Barcode Scanner Versions: This version of the 2D Barcode Scanner Breakout is physically identical to the second version (v2). Both the DE2120 on this breakout and the DE2290 on v2 function the same but they use different naming conventions for the command set. The silkscreen on this version reads "2D Barcode Scanner". Refer to the image below to make sure you are using the correct version:

Photo showing the two versions of the 2D Barcode Scanner

The SparkFun 2D Barcode Scanner Breakout is a nifty little breakout board featuring the DE2120 barcode scanner module from DYScan. The DE2120 reads 20 different barcode symbologies (both 1D and 2D) using a camera coupled with on-board image processing to identify and decode everything from UPC codes to QR codes. The module also features two LEDs: one for illumination and one to project the red line for "aiming" that you're used to seeing from laser-based scanners.

SparkFun 2D Barcode Scanner Breakout

SEN-18088
Retired

The breakout makes it easy to use the scanner module by connecting the scanner's USB serial output to a USB-C connector. The breakout also includes a standard 0.1"-spaced PTH header for the power, serial UART, trigger and status output connections. On top of that, we've added a trigger button, buzzer and status LED connected to the appropriate drive circuits to easily initialize scans and receive feedback from scanning barcodes.

Required Materials

You'll need a few things along with the 2D Barcode Scanner Breakout to follow this tutorial. You may not need everything though depending on what you have already so add anything you need from the items below to your cart.

The 2D Barcode Scanner Breakout can work as a USB device connected to a computer (PC or Single-Board like the Pi) with a USB Type-C cable.

Reversible USB A to C Cable - 2m

CAB-15424
$10.50

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

USB 2.0 Cable A to C - 3 Foot

CAB-15092
Retired

USB 2.0 C to C Cable - 1m

CAB-16395
Retired

If you want to use the 2D Barcode Scanner Breakout with a Pi, the options below can get you started:

Raspberry Pi 4 Model B (2 GB)

DEV-15446
$67.95

SparkFun Raspberry Pi 4 Basic Kit - 8GB

KIT-17980
Retired

Raspberry Pi 4 Model B (8 GB)

DEV-16811
$170.00

Raspberry Pi 3 B+

DEV-14643
$43.50

The breakout can also communicate with a microcontroller like an Arduino through the serial UART pins and other dedicated pins on the breakout's PTH header.

SparkFun Qwiic Pro Micro - USB-C

DEV-15795
$23.95

SparkFun RedBoard Qwiic

DEV-15123
$21.95

Arduino Uno - R3

DEV-11021
$27.60

SparkFun RedBoard Artemis

DEV-15444
$24.95

Using the breakout's PTH header requires some assembly and soldering. You may already have a few of these items but if not, the tools and hardware below will help with that assembly:

Soldering Iron - 60W (Adjustable Temperature)

TOL-14456
$25.95

Straight Header - Male (PTH, 0.1in., 40-Pin)

PRT-00116
$1.95

Hook-Up Wire - Assortment (Stranded, 22 AWG)

PRT-11375
$25.95

Solder Lead Free - 15-gram Tube

TOL-09163
$4.95

Recommended Reading

We would also recommend taking a look at the following tutorials if you aren't familiar with the concepts covered in them:

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.