ZX Distance and Gesture Sensor SMD Hookup Guide

≡ Pages
Contributors: Shawn Hymel, LightningHawk

Board Overview

The ZX Sensor works by bouncing infrared (IR) beams of light from the two LEDs on either side off of an object above the sensor. The bounced light returns to the receiver in the center of the sensor, and a microcontroller on the back of the sensor interprets the data. We can read the results using an I2C or UART connection.

Pin Descriptions

The ZX Sensor gives us two ports to connect to: I2C and UART. You can see both ports are broken out to the 0.1" thru holes. See the table below for a list of each pin and its function.

ZX FRONT

Pin LabelDescription
GRNNot used
TXOUART transmit out from the ZX Sensor
RXIUART receive. Not used at this time.
VCC3.3 - 5 V power supply
GNDConnect to ground
BLKNot used, but connected to GND
DRData Ready. High when there is data to be read via I2C
CLI2C clock
DAI2C data


Setting the Jumpers

The ZX Sensor has a couple of jumpers on the back of the board that can be opened or closed with a soldering iron.

ZX Sensor Back

I2C Pullups

The ZX Sensor, by default, comes with 4.7 kΩ pull-up resistors on the SDA and SCL I2C lines. Remove the solder on this jumper using solder wick to disconnect the pull-ups.

I2C Addr

By default, this jumper is open. Close it to change the I2C address of the sensor.

JumperI2C Address
Open0x10
Closed0x11