ZX Distance and Gesture Sensor Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

View the updated tutorial: ZX Distance and Gesture Sensor SMD Hookup Guide

≡ Pages
Contributors: Shawn Hymel

Resources and Going Further

After trying the basic ZX and gesture demos, you can try the other examples in the Arduino library. A description of each of the examples is given below:

  • I2C_Gesture_Demo -- Poll the sensor over I2C to see if any gestures have occurred.
  • I2C_Gesture_Interrupt -- The DR pin will go from low to high when a gesture is detected. This example reads the gesture over I2C and tells the sensor to clear DR.
  • I2C_ZX_Demo -- Poll the sensor periodically over I2C for Z- and X- axis data.
  • I2C_ZX_Interrupt -- The ZX Sensor will throw DR high whenever valid ZX data is ready.
  • UART_Gesture_Demo -- NOTE: Gestures over UART are not supported at this time. This demo is a placeholder for the time being.
  • UART_ZX_Demo -- Read Z- and X- axis data from a software serial port and display them on the Serial Monitor.

Here are some additional resources to help you with the ZX Sensor:

What will you make with the ZX Sensor? If you need some inspiration, check out these related tutorials:

Connecting Arduino to Processing

Send serial data from Arduino to Processing and back - even at the same time!

Serial Graphic LCD Hookup

Learn how to use the Serial Graphic LCD.

RGB Panel Hookup Guide

Make bright, colorful displays using the 32x16, 32x32, and 32x64 RGB LED matrix panels. This hookup guide shows how to hook up these panels and control them with an Arduino.

APDS-9960 RGB and Gesture Sensor Hookup Guide

Getting started guide for the Avago APDS-9960 color, proximity, and gesture sensor.