Comments: WiFly Shield Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #1457409 / about 8 years ago / 1

    The <a href="https://19216811.zone">ip address</a> doesn’t have a port number behind it as your does. Communicate with the Network section.

  • Astronomer / about 12 years ago / 1

    Just got my WiFly going again after a three year absence. Congratulations to Sparkfun on an excellent step-by step Hookup Guide - much better than it used to be. Just a remark here that might help others: I wasted a lot of time with the WiFly_RGB_LED_Server until I realised that my browser was blocking traffic between my laptop and the WiFly shield. Otherwise it would have worked first time. Thought number 2: the WiFly_RGB_LED_Server is rather slow. It takes about 12-15s from clicking say the Red button until the LED lights up. There is obviously a lot of slack here. For a previous server of mine the delay was only 3s but I was using an older library and the structure of my software was different. Thought number 3: It is possible to remove your router from the network by programming the RN-131C chip to operate as an "ad-hoc network" with a fixed IP address. This is easily done by following the Instructables website. You can then control your WiFly from a mobile phone, though there seems to be a problem with phones having the Android operating system.

  • Member #509015 / about 12 years ago / 1

    my case: arduino wireless Sd shield + Wifly RN-171. Following your tutorial everything works, even connection keep alive.etc.... BUT: the browser only shows transferring data (or waiting for 192.168.1.39 (my ardu-wlify ip)......the script ardu order: client.println("HTTP/1.1 200 OK"); doesnt appear in the browser...... :-( why? should the switch of the wireless shield be in micro or USB (it works on both)....should I connect something with wire? I just want to show a text in the browser from the ardu script via wireless..... any idea? many thanks

  • Member #509015 / about 12 years ago * / 1

    ->

  • RyanWV / about 13 years ago / 1

    When I verify the SpiUartTerminal code downloaded from the GitHub link and I get the error " 'SpiSerial' was not declared in this scope". I am using Arduino 1.0.5-r2. Should I use a previous version of Arduino to get this to work or should the code be modified and if so how?

    • Joel_E_B / about 13 years ago / 1

      Did you install the WiFly library?

      • Member #544018 / about 12 years ago / 1

        i had the same problem and i had import the wifly folder to the library. what should i do now?

  • Member #526209 / about 13 years ago / 1

    I followed the simple server example, but is not working, I uncommented the Serial.print(C) and I´m getting the following response:

    POST / HTTP/1.1 Host: 192.168.1.143:1050 Connection: keep-alive Content-Length: 7 Cache-Control: max-age=0 Accept: text/html,application+imip.n/10gi(NOl5HeC.1/Cyi--ee/.5pnddpg,,

    but besides that nothing else happens. What could be the problem? please help

    • Joel_E_B / about 13 years ago / 1

      It looks like you're not on port 80. You need to be on port 80 or a similar port that can handle HTTP requests.

      GET / HTTP/1.1 Host: 192.168.0.104

      Notice that my ip address doesn't have a port number behind it as your does. This is the first step in the Communicating with the Network section.


If you've found an issue with this tutorial content, please send us your feedback!