Voltage Dividers

≡ Pages
Contributors: jimblom

Introduction

A voltage divider is a simple circuit which turns a large voltage into a smaller one. Using just two series resistors and an input voltage, we can create an output voltage that is a fraction of the input. Voltage dividers are one of the most fundamental circuits in electronics. If learning Ohm's law was like being introduced to the ABC's, learning about voltage dividers would be like learning how to spell cat.

These are examples of potentiometers - variable resistors which can be used to create an adjustable voltage divider. We'll learn more about these soon.

Trimpot 10K Ohm with Knob

COM-09806
$1.25

Thumb Joystick

COM-09032
$5.25

Slide Pot - Small (10k Linear Taper)

COM-11620
$0.95

Rotary Potentiometer - Linear (10k ohm)

COM-09288
$1.25

Covered in this Tutorial

  • What a voltage divider circuit looks like.
  • How the output voltage depends on the input voltage and divider resistors.
  • How voltage dividers behave in the real-world.
  • Real-life voltage divider applications.

Suggested Reading

This tutorial builds on basic electronics knowledge. If you haven't already, consider reading these tutorials: