Vernier Shield Hookup Guide

≡ Pages
Contributors: bri_huang

Connecting an External Display

Adding an external display greatly enhances the ability to interface to the Vernier sensors independent of having a computer. The Arduino can be powered off a few AA batteries, and adding an LCD display will allow you to provide immediate feedback to the user.

What you'll need

Recommended Reading / Useful Resources

Getting Started

You'll need to solder on the male break-away headers to access pins D0 and D1. These will be used to transmit / send data to your Serial display device. You will also need to add headers to the power pins (5V and GND). We suggest using the female headers for this, though. Having power and GND exposed creates a risk of a short-circuit. Thankfully, the Arduino has a PTC resettable fuse that will protect your computer and the Arduino from this, but it should still be avoided.

The example code will vary depending on the Serial device you are using. You will need to connect Power (5V), GND, and the Transmit (Pin 1) on the Vernier Shield to your serial display device. Remember: the TX line should go to the RX line on the serial device.

Serial LCD Quickstart