Thing Plus Dual-Port Logging Shield Hookup Guide

≡ Pages
Contributors: Ell C, PaulZC

Example 6: Set Default Mode

If you run into a snag, setting things back to default is always a good way to go. This example will do just that!

Bring it on up in Arduino:

Where to find Example 6 in the menu

Having a hard time seeing the details? Click the image for a closer look.

Note: If you are using an Artemis Thing Plus, you will need to change Wire to Wire1 in the example code!

Make sure you've chosen the correct board and port (as seen in example 1) and then upload the code to your Thing Plus. When you open the Serial Monitor with the correct baud, you should see something like the following:

Example 6 output

Having a hard time seeing the details? Click the image for a closer look.