Thing Plus Dual-Port Logging Shield Hookup Guide

≡ Pages
Contributors: Ell C, PaulZC

Example 5: Sleep SPI

Example 5 shows the Sleep cycle for SPI mode. Bring up the example in Arduino:

Where to find Example 5 in the menu

Having a hard time seeing the details? Click the image for a closer look.

Note: If you are using an Artemis Thing Plus, you will need to change Wire to Wire1 in the example code!

Make sure you've chosen the correct board and port (as seen in example 1) and then upload the code to your Thing Plus. When you open the Serial Monitor with the correct baud, you should see something like the following:

Example 5 output

Having a hard time seeing the details? Click the image for a closer look.