THAT InGenius and OutSmarts Breakout Hookup Guide
Contributors:
Byron J.
Resources and Going Further
Now that you've successfully got your THAT 1206 and 1646 up and running, it's time to incorporate them into your own project!
Resources
For more information about the THAT InGenius and OutSmarts ICs, please refer to the datasheets and application notes below.
- THAT 1646 Datasheet
- THAT 1206 Datasheet
- Bill Whitlock's AES paper introducing the THAT 1200 family.
Going Further
For more information about balanced audio and sound system design, please refer to the following materials.
- Bill Whitlock is one of the leading experts on the subject of designing balanced audio interfaces. He has written many papers on the subject, including:
- Douglas Self's Small Signal Audio Design book is a great guide to audio circuitry in general.
- Norman Crowhurst's book of Audio Measurements explains how to quantify audio parameters such as frequency response, CMRR, and distortion.
- Discussion of the pin 1 problem
- Rane Application Note 110 is a very useful resource discussing the connection of balanced and unbalanced audio gear. Their App Note Library contains a number of other useful resources.
Need some inspiration for your next project? Check out some of these related tutorials:
Getting Started with the LilyPad MP3 Player
The LilyPad MP3 Player is an amazing little board that contains almost everything you need to play audio files. You can use it to create all kinds of noisy projects, from MP3 hoodies to talking teddy bears. Your imagination is the only limit! This tutorial will help you get started.
Sound Detector Hookup Guide
The Sound Detector is a microphone with a binary output. This guide explains how it works and how you can use it in your projects.
Hackers in Residence: The Sound Visualizer
A fun project that uses a Raspberry Pi and a custom Java app to create your own sound visualizer using a RGB LED matrix.
Hazardous Gas Monitor
Build a portable gas monitor to check for dangerous levels of hazardous gases.