TFMini - Micro LiDAR Module Hookup Guide

≡ Pages
Contributors: bboyho

Resources and Going Further

Now that you've successfully got your TFMini up and running, it's time to incorporate it into your own project! For more on the TFMini, check out the links below:

Need some inspiration for your next project? Check out some of these related tutorials:

VL6180 Hookup Guide

Get started with your VL6180 based sensor or the VL6180 breakout board.

Building an Autonomous Vehicle: The Batmobile

Documenting a six-month project to race autonomous Power Wheels at the SparkFun Autonomous Vehicle Competition (AVC) in 2016.

LIDAR-Lite v3 Hookup Guide

A tutorial for connecting the Garmin LIDAR-Lite v3 or the LIDAR-Lite v3HP to an Arduino to measure distance.

Qwiic Distance Sensor (RFD77402) Hookup Guide

The RFD77402 uses an infrared VCSEL (Vertical Cavity Surface Emitting Laser) TOF (Time of Flight) module capable of millimeter precision distance readings up to 2 meters. It’s also part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out how far away things are.