SX1509 I/O Expander Breakout Hookup Guide

≡ Pages
Contributors: jimblom

Installing the SparkFun SX1509 Arduino Library

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Now that you've got the hardware all mostly figured out, it's time to start programming! To help make using the SX1509 as painless as possible, we've written an Arduino library to help interface with it. Open the Arduino Library Manager and search for SparkFun SX1509. You can also manually install the SparkFun SX1509 Arduino Library from the GitHub repository by clicking on the button below to download the latest version of the library.

For help installing the library, check out our Installing an Arduino Library tutorial. If you downloaded the library as a ZIP, you can use Arduino's Sketch > Include Library > Add .ZIP Library tool to automatically add it to your Arduino sketchbook.

The SparkFun SX1509 Arduino library includes all sorts of examples, which demonstrate specific features of the I/O expander. Navigate to File > Examples > SparkFun SX1509 IO Expander to check them out.

SX1509 Library examples

Quickly, we'll walk you through a few quick examples that show off the I/O expander's range of features.