SparkFun Temperature Sensor - STTS22H (Qwiic) Hookup Guide

≡ Pages
Contributors: Ell C

Introduction

The SparkFun Temperature Sensor - STTS22H (Qwiic) and the SparkFun Micro Temperature Sensor - STTS22H (Qwiic) are Qwiic enabled breakout boards based on the ultralow-power, high-accuracy, digital temperature sensor STTS22H from ST Microelectronics. Thanks to its factory calibration the STTS22H offers high-end accuracy performance over the entire operating temperature range, reaching as low as ±0.5 °C without requiring any further calibration at the application level.

SparkFun Temperature Sensor - STTS22H (Qwiic)

SEN-21262
$6.95

SparkFun Micro Temperature Sensor - STTS22H (Qwiic)

SEN-21273
$8.53

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

Qwiic Connect System
Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.

What is an Arduino?

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

How to Install FTDI Drivers

How to install drivers for the FTDI Basic on Windows, Mac OS X, and Linux.

Using the Arduino Pro Mini 3.3V

This tutorial is your guide to all things Arduino Pro Mini. It explains what it is, what it's not, and how to get started using it.