SparkFun GPS Breakout (ZOE-M8Q and SAM-M8Q) Hookup Guide

≡ Pages
Contributors: Elias The Sparkiest

Which GNSS Unit Do I Pick?!

Size and GNSS Antenna

In each of the following Hardware Overview sections we layout the components and connections of each GNSS board. The SAM-M8Q comes in two different variations; a larger board with 1.6" x 1.6" dimensions and a compact version in the 1" x 1" standard Qwiic form-factor. The larger board dimensions provides a increases the ground plane area and performance of the embedded GNSS antenna; meanwhile, the smaller form-factor is more suitable for smaller project enclosures. The ZOE-M8Q also comes in the 1" x 1" standard Qwiic form-factor; however, it does not include an embedded GNSS antenna. Instead a U.FL connector is provided to connect to an external antenna. This offers more flexibility for users to attach their GNSS antenna outside of their project enclosure. The height of the ZOE-M8Q is also smaller than the compact 1" x 1" SAM-M8Q variant.

This picture shows the size difference between the GNSS products.
Difference in layout area between the GNSS boards.

This picture shows the height difference between the ZOE-M8Q and miniature SAM-M8Q variants
Difference in height between the compact SAM-M8Q (right) and ZOE-M8Q (left) boards.

GNSS Capability Comparison

The SAM-M8Q and ZOE-M8Q GNSS receivers both utilize the 72-channel u-blox M8 engine; therefore, their capabilities are so similar that the differences are negligible. The one major difference between them is that the SAM-M8Q does not connect to the Chinese BeiDou GNSS constellation.

ZOE-M8Q

GPS + GLONASS GPS GLONASS Galileo BeiDou
Horizontal Position Accuracy 2.5m 2.5m 4m 3m 3m
Max Navigation Update Rate 10Hz 18Hz 18Hz 18Hz 18Hz
Time-To-First-Fix Cold Start 26s 29s 30s 45s 34s
Hot Start 1s 1s 1s 1s 1s

SAM-M8Q

GPS + GLONASS GPS GLONASS Galileo BeiDou
Horizontal Position Accuracy 2.5m 2.5m 8m TBD N/A
Max Navigation Update Rate 10Hz 18Hz 18Hz 18Hz N/A
Time-To-First-Fix Cold Start 26s 29s 30s TBD N/A
Hot Start 1s 1s 1s TBD N/A

SPI Interface

Both GNSS receivers support I2C and serial communication to receive your NMEA data. However, the ZOE-M8Q also supports a SPI interface. The SPI interface can be enabled by closing the SPI jumper on the bottom of the board.

This picture shows the SPI jumper and header on the underside of the ZOE-M8Q board.