SparkFun expLoRaBLE Hookup Guide

≡ Pages
Contributors: QCPete, santaimpersonator

Peer-to-Peer Example

Note: This section has been updated to no longer use the modified RadioLib library. As mentioned in the pull request for our changes, users only need to delcare that the SPI1 bus is used.

Important: Users should also use the example codes that we provide with the download buttons below. There seem to be several users, trying to use the built-in examples and running into issues, even though we provide example codes below. The example codes below have been written and tested for users to be able to upload directly to their expLoRaBLE and execute without any issues. (Obviously because we are based in th US, the example code has been written for use at 915MHz (the reserved frequency band for our region). Users outside the US and using a different frequency band, will need to reference the library and modify the code on their own.)

In this example, the RadioLib library utilizes the frequency shift keying (FSK) capabilities of the SX1262 transceiver. For this example, users will need two expLoRaBLEs; one to transmit data and the other to receive that data. For more information on this library, check out the GitHub repository Wiki. User simply need to download and upload the code below to separate expLoRaBLEs:

Once the example codes has been uploaded to their respective boards, users should see the data transmissions in the Serial Monitor:

Serial Monitor- Transmitter Output
A screen shot of the Serial Monitor, showing that data is being transmitted. (Click to enlarge)

Serial Monitor- Receiver Output
A screen shot of the Serial Monitor, showing that data was received. (Click to enlarge)

Note: The Arduino IDE only lets users connect to one COM (or serial) port at a time. Just verify that the board with the transmit code is sending data; then, monitor the COM port of the board with the receiver code for incoming data. If all is working, Hello World! transmissions will begin to appear.