Comments: SparkFun expLoRaBLE Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #1697553 / about 5 years ago * / 1

    The modified transmit sketch in the Peer-to-Peer Example has an error. All lines that contain: else if (state = ERR...) must be changed to else if (state = RADIOLIB_ERR...) in order to function correctly with the RadioLib library.

  • Member #728158 / about 5 years ago / 1

    Does the semtech chip in this device support 8 channels or only one?

  • Member #1693662 / about 5 years ago / 1

    How can I access to "secondary" UART module by using TX/RX pin on the board? I thought that I could access it in the same way as "Serial1" of Arduino Mega, but It didn't work.

    • santaimpersonator / about 5 years ago / 2

      Please, refer to this supplementary tutorial for using the Apollo3 based MCUs in the Arduino IDE, it contains an example for using other serial ports. From the example code:

      You can create new UART objects (which inherit from the HardwareSerial class in Arduino) by specifying the TX and RX pins, and optionally the RTS and CTS pins to enable flow control. Here are the constructor prototypes: UART(PinName tx, PinName rx, PinName rts, PinName cts); UART(pin_size_t tx, pin_size_t rx, pin_size_t rts, pin_size_t cts);

  • Member #1680478 / about 5 years ago / 1

    I'm trying to add my device in "The Thing Stack" and one parameter require is the LoRaWAN version, but I was not able to find it in the datasheet. Which version is in use in the SparkFun expLoRaBLE?

    • santaimpersonator / about 5 years ago / 1

      I'm not too familiar with the Things Stack. They transitioned over, shortly after this tutorial was written.

      That being said, it sounds like you are adding a device with the OTAA method, which is outside the scope of the tutorial (we only cover the ABP method). It should be noted, that information isn't provided because it would only be available with an end-user commercial product (as far as I can gather). Therefore, the LoRaWAN version would be based on the firmware (i.e. code) that you program the board with... since that would control how it responds/behaves as a device on the network.

  • Member #133466 / about 6 years ago / 1

    Does anyone know if this works with the Helium network?

    • santaimpersonator / about 6 years ago / 1

      We have not tested this board directly with the Helium network. However, the information on their site seems to indicate that the board would be compatible.

    • ElephantHat / about 6 years ago / 1

      I haven't tested but I don't see why it wouldn't work. It's not as simple as pushing a few buttons but there's a document that explains what you need to do to convert it over from TTN to Helium.

      https://docs.helium.com/use-the-network/console/migrating-devices/

  • ElephantHat / about 6 years ago * / 1

    I'm trying to run the code after making all the necessary changes. I'm getting an error on line 79: exit status 1 'D36' was not declared in this scope

    I am new to Arduino programming, but I think I need to change these values to match the board but I can't find that documentation anywhere. So I'm wondering, am I doing something else wrong?


    Figured it out. You have to go to tools --> Board --> Sparfun apollo3 --> and select the LoRa Thing plus explorable

    • santaimpersonator / about 6 years ago / 1

      Glad to hear that you were able to figure out a solution on your own.

  • Member #266582 / about 6 years ago / 1

    Is anyone else having problems getting Serial1 working on Arduino? As I look at the schematic, I see that the module is using GPIO 18 for TX, and GPIO 19 for RX. However, looking at the Serial example provided, this isn't a valid pair. It seems to be 18,15 or 20,19. Am I missing something?


If you've found an issue with this tutorial content, please send us your feedback!