smôl ZOE-M8Q Hookup Guide

≡ Pages
Contributors: PaulZC

Hardware Overview

In this section we'll cover what's included on the smôl ZOE-M8Q Peripheral Board.

GNSS Capabilities

The u-blox ZOE-M8Q is able to connect to up to three different GNSS constellations at a time making it very accurate for its size.

smôl ZOE-M8Q and support components

Below are the listed capabilities of the GNSS unit:

GNSS GPS and GLONASS GPS GLONASS BeiDou Galileo
Horizontal Position Accuracy 2.5m2.5m4m3m3m
Max Navigation Update Rate ROM 10Hz 18Hz 18Hz 18Hz 18Hz
Flash 5Hz 10Hz 10Hz 10Hz 10Hz
Time-To-First-Fix Cold Start 26s 29s 30s 34s 45s
Hot Start 1s 1s 1s 1s 1s
SensitivityTracking and Navigation -167dBm -166dBm -166dBm -160dBm -159dBm
Reacquisition -160dBm -160dBm -156dBm -157dBm -153dBm
Cold Start-148dBm -148dBm -145dBm -143dBm -138dBm
Hot Start -157dBm -157dBm -156dBm -155dBm -151dBm
Velocity Accuracy 0.05m/s
Heading Accuracy 0.3 degrees

Power

Power for this board - and all smôl boards - should be 3.3V.

Battery

The small metal disk in the center of the board is a small lithium battery. This battery does not provide power to the IC like the 3.3V system does, but to relevant systems inside the IC that allow for a quick reconnection to satellites. The time to first fix will be about ~29 seconds, but after the product has a lock, that battery will allow for a one second time to first fix. This is known as a hot start and lasts for four hours after the board is powered down. The battery provides over a year's worth of power to the backup system and charges slowly when smôl 3.3V is powered.

smôl ZOE-M8Q backup battery

Jumpers

There is only one jumper on the top of this product, labelled V_ANT. By default, 3.3V power is provided on the u.FL connector for an active antenna. Cutting the V_ANT jumper disconnects the 3.3V power.

This is a picture of the board with the V_ANT jumper highlighted.

u.FL Connector

The u.FL connector on the board is where you will plug in your antenna. This is a compact connector for RF antennas, that has the same function as the traditional SMA connector. You may be more familiar and even own some antennas that use SMA connectors; never fear, we carry a U.FL to SMA cable adapter. Check out our tutorial on using U.FL connectors, if this is your first.

Pictured is the small u.FL connector

Power Switching

The smôl ZOE-M8Q includes an on-board power switch (MOSFET):

smôl ZOE-M8Q power switch

Power for the ZOE-M8Q is controlled via the smôl GPIO0 signal. Leave GPIO0 floating or pull high to disable power to the ZOE-M8Q (default state). Pull the smôl GPIO0 signal low to enable power for the ZOE-M8Q.

FPC Connections

Like all of our smôl boards, the ZOE-M8Q Peripheral Board is equipped with two 16-way 0.5mm-pitch Flexible Printed Circuit connectors. FPCs are used to link the smôl boards together in a daisy-chain.

The pin-out for the smôl ZOE-M8Q IN connector is as follows:

IN Connector Pin No.Signal NameFunctionNotes
1PROC_PWR_ENProcessor Power EnableNot used
23V33.3V Power Rail
3GNDPower Ground / 0V
4SCLKSPI ClockNot used
5COPISPI Controller Out Peripheral InNot used
6CIPOSPI Controller In Peripheral OutNot used
7CS0SPI Chip Select 0Not used
8CS1SPI Chip Select 1Not used
9CS2SPI Chip Select 2Not used
10GPIO0ZOE-M8Q Power ControlPull low to enable power for the ZOE-M8Q
11GPIO1General Purpose Input / Output 1Connected to Pin 10 (GPIO0) on the OUT connector
12SDAI2C DataUsed for ZOE-M8Q communication
13SCLI2C ClockUsed for ZOE-M8Q communication
14GNDPower Ground / 0V
153V33.3V Power Rail
16V_USBUSB Power Rail (5V)Not used

The pin-out for the smôl ZOE-M8Q OUT connector is as follows:

OUT Connector Pin No.Signal NameFunctionNotes
1PROC_PWR_ENProcessor Power EnableNot used
23V33.3V Power Rail
3GNDPower Ground / 0V
4SCLKSPI ClockNot used
5COPISPI Controller Out Peripheral InNot used
6CIPOSPI Controller In Peripheral OutNot used
7CS0SPI Chip Select 0Not used
8CS1SPI Chip Select 1Not used
9CS2SPI Chip Select 2Not used
10GPIO0General Purpose Input / Output 0Connected to Pin 11 (GPIO1) on the IN connector
11GPIO1Not connected
12SDAI2C DataUsed for ZOE-M8Q communication
13SCLI2C ClockUsed for ZOE-M8Q communication
14GNDPower Ground / 0V
153V33.3V Power Rail
16V_USBUSB Power Rail (5V)Not used

We use a technique called waterfalling on the GPIO signals. If you haven't used waterfalling before, please check out the smôl Hookup Guide.