Si4703 FM Radio Receiver Hookup Guide

≡ Pages
Contributors: Toni_K

Introduction

Heads up! This tutorial was written for Si4703 FM Tuner Evaluation Board V13 (WRL-12938). The 3.3V and GND pins are switched in the new revision. Make sure you connect to the correct pins for power if you are using an older version like V11 (WRL-10663) or the breakout board.

The Si4703 FM tuner evaluation breakout board enables you to tune in to FM radio stations, using the Si4703 FM tuner chip from Silicon Laboratories. This IC also works well for filter and carrier detection, and enables data such as the station ID and song name to be displayed to the user.

SparkFun FM Tuner Evaluation Board - Si4703

WRL-12938
$26.50

Required Materials

You will need the following materials to work on this project.

Keep in mind you will also need standard soldering materials to complete this tutorial, as well as either a set of speakers or headphones with a 3.5mm jack to plug into the Si4703 board.

Suggested Reading

If you aren't familiar with any of the concepts below, check out these links and get caught up before moving ahead with the Si4703.

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

How to Power a Project

A tutorial to help figure out the power requirements of your project.

Working with Wire

How to strip, crimp, and work with wire.

Using GitHub to Share with SparkFun

A simple step-by-step tutorial to help you download files from SparkFun's GitHub site, make changes, and share the changes with SparkFun.

Using the Arduino Pro Mini 3.3V

This tutorial is your guide to all things Arduino Pro Mini. It explains what it is, what it's not, and how to get started using it.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.