Setting up a Raspberry Pi 3 as an Access Point

≡ Pages
Contributors: Shawn Hymel

Introduction

Note: This tutorial was based on instructions found on this blog.

The Raspberry Pi 3 comes with a built-in wireless adapter, which makes it easy to configure it as a WiFi hotspot to share Internet or host your own internal web site. The first part of this guide will show you how to set up the Pi to broadcast its SSID, accept WiFi connections, and hand out IP addresses (using DHCP). The next section shows you how to enable a pass-through Ethernet connection should you want to share your Internet connection.

Raspberry Pi 3 B+

DEV-14643
$43.50

Before You Get Started!

You will want a Raspberry PI 3 or Raspberry Pi Zero W along with any hookup accessories you might need (for example, a power adapter and micro SD card).

You will want to load an operating system (OS) onto the SD card and be able to log into the Pi and open a terminal.

Note: This tutorial was created with Raspbian Stretch (version: March 2018). Using a different version may require performing different steps than what's shown in this tutorial. If you would like to download the March 2018 version of Raspbian, it can be found below.

Raspbian Stretch (version: March 2018) Download (ZIP)

If you need help installing an OS onto the Raspberry Pi, these tutorials can be helpful:

Suggested Reading

If you aren't familiar with the following concepts, we recommend checking out these tutorials before continuing.

Raspberry Pi 3 Starter Kit Hookup Guide

Guide for getting going with the Raspberry Pi 3 Model B and Raspberry Pi 3 Model B+ starter kit.

Getting Started with the Raspberry Pi Zero Wireless

Learn how to setup, configure and use the smallest Raspberry Pi yet, the Raspberry Pi Zero - Wireless.

Headless Raspberry Pi Setup

Configure a Raspberry Pi without a keyboard, mouse, or monitor.

Set Up WiFi Access Point

Make sure your Raspberry Pi is connected to the Internet. Open a terminal window (either in a console window or over a serial/SSH connection).

Install Packages

To install the required packages, enter the following into the console:

language:bash
sudo apt-get -y install hostapd dnsmasq

Hostapd is a program that allows you to use the WiFi radio as an access point, and Dnsmasq is a lightweight combination of DHCP and DNS services (handing out IP addresses and translating domain names into IP addresses).

Set Static IP Address

In recent versions of Raspbian, network configuration is managed by the dhcpcd program. As a result, we'll need to tell it to ignore the wireless interface, wlan0, and set a static IP address elsewhere.

Note: If you are connected to your Raspberry Pi using SSH over wireless, you will want to connect with a keyboard/mouse/monitor, Ethernet, or serial instead until we get the access point configured.

Edit the dhcpcd file:

language:bash
sudo nano /etc/dhcpcd.conf

Scroll down, and at the bottom of the file, add:

language:bash
denyinterfaces wlan0

Your terminal window should look similar to the image below.

Prevent dhcpcd from configuring wlan0

Save and exit by pressing ctrl + x and y when asked.

Next, we need to tell the Raspberry Pi to set a static IP address for the WiFi interface. Open the interfaces file with the following command:

language:bash
sudo nano /etc/network/interfaces

At the bottom of that file, add the following:

language:bash
auto lo
iface lo inet loopback

auto eth0
iface eth0 inet dhcp

allow-hotplug wlan0
iface wlan0 inet static
    address 192.168.5.1
    netmask 255.255.255.0
    network 192.168.5.0
    broadcast 192.168.5.255

Your terminal window should look similar to the image below.

Set WiFi static IP address in the Raspberry Pi's interfaces file

Save and exit by pressing ctrl + x and y when asked.

Configure Hostapd

We need to set up hostapd to tell it to broadcast a particular SSID and allow WiFi connections on a certain channel. Edit the hostapd.conf file (this will create a new file, as one likely does not exist yet) with this command:

language:bash
sudo nano /etc/hostapd/hostapd.conf

Enter the following into that file. Feel fee to change the ssid (WiFi network name) and the wpa_passphrase (password to join the network) to whatever you'd like. You can also change the channel to something in the 1-11 range (if channel 6 is too crowded in your area).

language:bash
interface=wlan0
driver=nl80211
ssid=MyPiAP
hw_mode=g
channel=6
ieee80211n=1
wmm_enabled=1
ht_capab=[HT40][SHORT-GI-20][DSSS_CCK-40]
macaddr_acl=0
auth_algs=1
ignore_broadcast_ssid=0
wpa=2
wpa_key_mgmt=WPA-PSK
wpa_passphrase=raspberry
rsn_pairwise=CCMP

Your terminal window should look similar to the image below.

Configure Hostapd

Save and exit by pressing ctrl + x and y when asked.

Unfortunately, hostapd does not know where to find this configuration file, so we need to provide its location to the hostapd startup script. Open /etc/default/hostapd:

language:bash
sudo nano /etc/default/hostapd

Find the line #DAEMON_CONF="" and replace it with:

language:bash
DAEMON_CONF="/etc/hostapd/hostapd.conf"

Your terminal window should look similar to the image below.

Configure Hostapd to load the .conf file on boot

Save and exit by pressing ctrl + x and y when asked.

Configure Dnsmasq

Dnsmasq will help us automatically assign IP addresses as new devices connect to our network as well as work as a translation between network names and IP addresses. The .conf file that comes with Dnsmasq has a lot of good information in it, so it might be worthwhile to save it (as a backup) rather than delete it. After saving it, open a new one for editing:

language:bash
sudo mv /etc/dnsmasq.conf /etc/dnsmasq.conf.bak
sudo nano /etc/dnsmasq.conf

In the blank file, paste in the text below. Note that we set up DHCP to assign addresses to devices between 192.168.5.100 and 192.168.5.200. Remember that 192.168.5.1 is reserved for the Pi. So, anything between 192.168.5.2 - 192.168.5.9 and between 192.168.5.201 - 192.168.5.254 can be used for devices with static IP addresses.

language:bash
interface=wlan0 
listen-address=192.168.5.1
bind-interfaces 
server=8.8.8.8
domain-needed
bogus-priv
dhcp-range=192.168.5.100,192.168.5.200,24h

Your terminal window should look similar to the image below.

Set up dnsmasq with DHCP on WiFi

Save and exit by pressing ctrl + x and y when asked.

Test WiFi connection

Restart the Raspberry Pi using the following command:

language:bash
sudo reboot

After your Pi restarts (no need to log in), you should see MyPiAP appear as a potential wireless network from your computer.

Raspberry Pi broadcasting its WiFi network

Connect to it (the network password is raspberry, unless you changed it in the hostapd.conf file). Open a terminal on your computer and enter the command ipconfig (Windows) or ifconfig (Mac, Linux). You should see that you have been assigned an IP address in the 192.168.5.100 - 192.168.5.200 range.

Here's an example of what you may see after connecting wirelessly to the Pi.

IP address assigned by the DHCP server on the Raspberry Pi

If you just want to use the Pi as a standalone WiFi access point, you can stop here. If you want to connect it to another network (over Ethernet) in order to share Internet (much like a WiFi router), continue on.

Enable Packet Forwarding

We can use the Raspberry Pi as a router by being able to connect it to another network over Ethernet and have WiFi-connected devices be able to talk to that network. By doing this, we can share an Internet connection from the Pi.

Configure NAT

Make sure you are logged into your Pi. Edit the /etc/sysctl.conf file:

language:bash
sudo nano /etc/sysctl.conf

Look for the line #net.ipv4.ip_forward=1, and uncomment it by deleting the #.

language:bash
net.ipv4.ip_forward=1

Your terminal window should look similar to the image below.

Enable IPv4 packet forwarding

Save and exit by pressing ctrl + x and y when prompted.

Finally, we need to configure Network Address Translation (NAT) between the Ethernet and WiFi interfaces to allow devices on both networks to communicate with each other. In the terminal, enter the following:

language:bash
sudo iptables -t nat -A POSTROUTING -o eth0 -j MASQUERADE  
sudo iptables -A FORWARD -i eth0 -o wlan0 -m state --state RELATED,ESTABLISHED -j ACCEPT
sudo iptables -A FORWARD -i wlan0 -o eth0 -j ACCEPT

This will work for now, but on reboot, the Pi will revert back to its previous state. To fix this, we need these NAT rules to be applied each time it starts up. Save the current rules to a file with this command:

language:bash
sudo sh -c "iptables-save > /etc/iptables.ipv4.nat"

Linux provides us with a number of ways to run commands on boot. Usually, the easiest is to put those commands into the /etc/rc.local script. To have our NAT rules restored on boot, we edit the rc.local file:

language:bash
sudo nano /etc/rc.local

Just above the exit 0 line (which ends the script), add the following:

language:bash
iptables-restore < /etc/iptables.ipv4.nat 

Your terminal window should look similar to the image below.

Restore NAT rules during boot with rc.local

Save and exit by pressing ctrl + x and y when prompted.

Test It Out

Restart your Pi:

language:bash
sudo reboot

Give your Pi a couple minutes to restart (once again, no need to log in). Connect an Ethernet cable from your Internet router (or switch, etc.) to your Pi. Once the Pi has started, connect to the MyPiAP network from your computer. Open a web browser, and navigate to the website of your choice.

Example of a good website

You can also open a terminal on your computer and ping a known Internet address (e.g. 8.8.8.8 is one of Google's Public DNS servers).

Ping 8.8.8.8 over the Raspberry Pi WiFi network

Resources and Going Further

With the Raspberry Pi set up as an access point, you can now configure it to host a web site (e.g. using Apache), share drive space (e.g. Samba), and any other fun router customizations you might want (but on a Pi, instead!).

Looking for some inspiration for your Raspberry Pi? Check out these tutorials:

Raspberry Pi Twitter Monitor

How to use a Raspberry Pi to monitor Twitter for hashtags and blink an LED.

Raspberry gPIo

How to use either Python or C++ to drive the I/O lines on a Raspberry Pi.

Raspberry Pi Zero Helmet Impact Force Monitor

How much impact can the human body handle? This tutorial will teach you how to build your very own impact force monitor using a helmet, Raspberry Pi Zero, and accelerometer!

Setting Up the Pi Zero Wireless Pan-Tilt Camera

This tutorial will show you how to assemble, program, and access the Raspberry Pi Zero as a headless wireless pan-tilt camera.

Using Flask to Send Data to a Raspberry Pi

In this tutorial, we'll show you how to use the Flask framework for Python to send data from ESP8266 WiFi nodes to a Raspberry Pi over an internal WiFi network.

Raspberry Pi Stand-Alone Programmer

This tutorial will show you how to use a headless Raspberry Pi to flash hex files onto AVR microcontrollers as a stand-alone programmer. It also tells the story about production programming challenges, how SparkFun came to this solution, and all the lessons learned along the way.

Interested in learning more about WiFi?

Get a background in how WiFi works as well as the hardware available to help you connect your project wirelessly.

Take me there!
Learn About WiFi