RGB Panel Jumbotron

≡ Pages
Contributors: b_e_n

Hardware Hookup

Here are the pin connections between LED panel connector and the Teensy 3.1:

Panel Pin LabelPanel Connector Pin #Arduino PinNotes
R012Red data (columns 1-16)
G0214Green data (columns 1-16)
B037Blue data (columns 1-16)
GND4GNDGround
R158Red data (columns 17-32)
G166Green data (columns 17-32)
B1720Blue data (columns 17-32)
GND8GNDGround
A915Demux input A0
B1022Demux input A1
C1123Demux input A2
D129Demux input E1, E3 (32x32 panels only)
CLK1310LED drivers' clock
STB1413LED drivers' latch
OE1511LED drivers' output enable
GND16GNDGround


Panel connector pin numbering convention: Pin 1 is top left (R0), pin 2 is to the right of pin 1, pin 3 is below pin 1, pin 4 is to the right of pin 3, etc. Pin 16 is the bottom right.

And for handy reference, here's a pinout chart for the Teensy 3.1:

alt text

When connecting into the ribbon cable connector, pay attention to the notch that signifies polarity. When looking at the cable with the notch facing up and on the left side, R0 (pin 1) should be at the top left.

Red, green, and blue wires inserted into cable

Both red and blue wires should be on the notch side, the greens should be on the other.

alt text

Your hardware hookup should look something like this when you're done.