Qwiic Distance Sensor (VL53L1X) Hookup Guide
This Tutorial is Retired!
This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.
View the updated tutorial: Qwiic Distance Sensor (VL53L1X, VL53L4CD) Hookup Guide
Contributors:
Englandsaurus
Resources and Going Further
Now that you've successfully got your Qwiic Distance Sensor up and running, it's time to incorporate it into your own project!
For more information, check out the resources below:
- Schematic (PDF)
- Eagle Files (ZIP)
- VL53L1X Datasheet
- VL53L1X User Manual
- GitHub Repos:
- SparkFun Product Showcase: VL53L1X Qwiic Distance Sensor
- Qwiic Landing Page
Want a great use case for your ToF sensor? How about integrating one into your AVC submission? Have a look here:
Need even more inspiration for your next project? Check out some of these related tutorials:
Qwiic HAT for Raspberry Pi Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi. This Qwiic connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors.
Qwiic VR IMU (BNO080) Hookup Guide
Figure out how things are oriented with the robust 9 degrees of freedom (DOF) BNO080 IMU. Maybe even make your own virtual reality (VR) applications if you're feeling savvy.
Qwiic MultiPort Hookup Guide
The SparkFun Qwiic MultiPort adds additional ports to boards that have only one Qwiic port on their I2C bus. Once added, you can use it as a hub to add as many I2C devices to the bus as you need! You can also use the board as an alternative to a daisy chained configuration.
Qwiic LED Stick - APA102C Hookup Guide
Add some I2C RGB to your project with the SparkFun Qwiic LED Stick - APA102C
Or check out this blog post for more ideas!