Qwiic Distance Sensor (VL53L1X) Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

View the updated tutorial: Qwiic Distance Sensor (VL53L1X, VL53L4CD) Hookup Guide

≡ Pages
Contributors: Englandsaurus

Hardware Overview

First let's check out some of the characteristics of the VL53L1X sensor we're dealing with, so we know what to expect out of the board.

CharacteristicRange
Operating Voltage2.6V-3.5V
Power Consumption20 mW @10Hz
Measurement Range~40mm to 4,000mm
Resolution+/-1mm
Light SourceClass 1 940nm VCSEL
I2C Address0x29
Field of View15° - 27°
Max Read Rate50Hz

Pins

The following table lists all of the VL53L1X's pins and their functionality.

PinDescriptionDirection
GNDGroundIn
3.3VPowerIn
SDADataIn
SCLClockIn
INTInterrupt, goes low when data is ready.Out
SHUTShutdown, can be pulled low to put the IC in shutdown mode.In

Optional Features

The VL53L1X breakout has pull up resistors attached to the I2C bus as well as the interrupt pin; if multiple sensors are connected to the bus with the pull-up resistors enabled, the parallel equivalent resistance will create too strong of a pull-up for the bus to operate correctly. As a general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected to the bus. If you need to disconnect the pull up resistors they can be removed by cutting the traces on the corresponding jumpers highlighted below.

Pullup Jumpers

The onboard LED (highlighted below) will light up when the board is powered, and the sensor (also highlighted below) should be left uncovered in your application.

Sensor and LED