Preassembled 40-pin Pi Wedge Hookup Guide

≡ Pages
Contributors: Byron J.

Assembly

Contents

The Preassembleed Pi Wedge comes with the Wedge PCB, and a 40-pin ribbon cable.

Connection

The 40-pin ribbon cable is used to connect the wedge to the Pi. This cable is polarized — notice that the pin 1 marking is very subtle. On the Pi Wedge PCB end, the tooth on the cable will interface with the notch in the shrouded header. Insert the IDC cable into the Pi Wedge's polarized connector so that the cable extends away from the breadboard connection.

alt text

Inserting the ribbon cable

Insert the Wedge into the center of the breadboard so that each pin has their own row.

alt text

Wedge inserted in breadboard.

The header on the Pi itself doesn't have anything to help guarantee the alignment. You'll need to take care that it gets connected properly. Pin 1 on the Pi is marked with a dog-eared corner on the silkscreened rectangle. The ribbon cable connector is embossed with (a barely visible) small triangle that marks pin 1. The first pin is also coded on the wire, such as the red markings in the photo below (though it may also be another color, such as black or dark blue). Insert the IDC cable to the Pi so that the cable extends away from the Pi.

Proper Orientation for the IDC Cable on the Pi

Proper pin-1 orientation

If you decide to connect to the Pi using serial, you can insert a 3.3V FTDI to the Pi Wedge. The FTDI connector needs to be aligned correctly. Be sure to match up the "GRN" and "BLK" markings on both boards.

FTDI connected to Pi Wedge

Proper 3.3V FTDI-Basic orientation

Your setup will look similar to the image below. In this case, we used a Pi 3 in an enclosure.

Pi Wedge Setup with Pi

In the next section, we'll explore how the signals from the Pi are mapped to the Wedge.