MPU-9250 Hookup Guide
Resources and Going Further
For more information about the MPU-9250 Breakout, check out the links below.
Many of the advanced features of the MPU-9250 are only accessable by agreeing to a pages of licensing terms and logging in as a developer to get access to Embedded MotionDriver 6.12. This approach isn't super Arduino friendly. At power up 3062 bytes of undocumented hex needs to be loaded into the MPU-9250.
#define DMP_CODE_SIZE (3062)
static const unsigned char dmp_memory[DMP_CODE_SIZE] = {
/* bank # 0 */
0x00, 0x00, 0x70, 0x00, 0x00, 0x00, 0x00, 0x24, 0x00, 0x00, 0x00, 0x02, 0x00, 0x03, 0x00,
0x00, 0x00, 0x65, 0x00, 0x54, 0xff, 0xef, 0x00, 0x00, 0xfa, 0x80, 0x00, 0x0b, 0x12, 0x82,...
That binary combined with the driver and any code that does something with the sensor data quickly maxes out smaller microcontrollers. Feel free to register and play around if you want to take this product further.
A customer of ours shared his great tutorial on Affordable 9-DoF Sensor Fusion. Check it out for more info on sensor fusion.
For more SparkFun sensor fun, check out these other great tutorials. (This was fun, right??)
BadgerHack: Sensor Add-On Kit
Qwiic Accelerometer (MMA8452Q) Hookup Guide
SparkFun Inventor's Kit Experiment Guide - v4.1
SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide
Or check out this blog post for ideas: