MPU-9250 Hookup Guide

≡ Pages
Contributors: .Brent.

Hardware Connections

The MPU-9250 breakout board runs on 3.3 VDC, so a 3.3V USB to UART bridge such as the SparkFun FTDI Basic Breakout - 3.3V or the SparkFun Beefy 3 - FTDI Basic Breakout can be used to power and bridge communication with a micro controller. In this case an Arduino Pro Mini 328 - 3.3V/8MHz was chosen so logic level translation isn't needed.

Fritzing Diagram of MPU-9450 Connected to Arduino

Fritzing diagram of setup

Only 4 connections are needed for I2C communication.

Snapped PCB next to 0.1" header

Minimum parts for a breadboard compatible setup

For stability in the breadboard, another four pins were soldered on: VDDIO, AD0/SDO, CS, and INT.

PCB with breadboard compatible male headers soldered on

PCB with breadboard compatible male headers soldered on

Here is the final setup used for testing.

Setup used for testing

Setup used for testing