Comments: MicroView Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #834734 / about 7 years ago / 1

    in example 4 when i copy the code to arduino it says;

    error: no matching function for call to 'MicroView::drawBitmap(uint8_t [384])

    why is this? please help

    • santaimpersonator / about 7 years ago / 1

      Hi there, it sounds like you are looking for technical assistance. Please use the link in the banner above, to get started with posting a topic in our forums. Our technical support team will do their best to assist you.

  • Member #1024203 / about 9 years ago / 1

    What are the steps to get the operating voltage for MicroView to 3.3 V , I have a sensor that communicates using I2C but it's operating voltage is 3.3V.

    • Joel_E_B / about 9 years ago / 1

      You cannot change the operating voltage of the MicroView as it needs 5V for the OLED screen. However, you can use a logic level converter to connect the MicroView to 3.3V devices without damaging the attached device(s). That said, we often hook up 3.3V I2C devices and 5V I2C devices to one another with no issues since I2C is an open drain technology meaning that I2C master and slave devices can only drive these lines low or leave them open.

  • -------------------- Tech Support Tips/Troubleshooting/Common Issues --------------------

    Resources

    If you have not checked out the MicroView kit's tutorials, try checking out the online tutorials for the kit:

     

    Going Further

    Try using a ESP8266, Logic Level Converter, and a Serial Protocol to display the current weather on a MicroView. This tutorial might be of some use using Yahoo's Weather API:

  • Member #716737 / about 10 years ago / 1

    In the c file it is called CMD_DRAWBITMAP with one comment line. // TODO

    I think this is called a failure to test completely.

  • Member #644832 / about 10 years ago / 1

    In Example 4 - Drawing bitmaps I'm getting an error on line "uView.drawBitmap(bender);" The error message: no matching function for call to 'MicroView::drawBitmap(uint8_t[348])'

    Please help

    • Joel_E_B / about 10 years ago / 1

      I found the issue. The drawBitmap function was added to the MicroView library several months ago. However, I failed to update the tree on GitHub from which the Arduino Library manger pulls the library files. I will fix this when I get a chance. In the meantime, you can pull my version of the library directly from GitHub, here and install it manually vs through the library manger to get the drawButmap function to work properly.

      • Joel_E_B / about 10 years ago / 1

        Ok, the library has been updated and pushed to the Arduino Library manager. Please install the SparkFun MicroView library version 1.0.2, which has the drawBitmap function.

        • Member #306393 / about 8 years ago / 1

          I am getting the "no matching function error" Arduino 1.8.9 and Sparkfun Microview 1.0.2 is the installed version.

          Any idea what's going on?


If you've found an issue with this tutorial content, please send us your feedback!