MicroMod Weather Carrier Board Hookup Guide

≡ Pages
Contributors: El Duderino, MAKIN-STUFF

Resources and Going Further

For more information about the MicroMod Weather Carrier Board, check out the following links:

For more information about the SparkFun MicroMod Ecosystem, take a look at the links below:

Looking for some project inspiration using your Weather Station Carrier? The tutorials below can help you get started!

MS5803-14BA Pressure Sensor Hookup Guide

Breakout of MS5803-14BA Pressure Sensor to measure the absolute pressure of the fluid around them to determine altitude, water depth, or any other tasks that require an accurate pressure reading. This includes air, water, and anything else that acts like a viscous fluid.

MPL3115A2 Pressure Sensor Hookup Guide

Getting started with the MPL3115A2 Pressure Sensor.

SparkFun gator:UV Hookup Guide

The gator:UV is an I2C based UV sensor. This tutorial will get you started using the gator:UV with the micro:bit platform.

SparkFun AS3935 Lightning Detector Hookup Guide (v20)

Are you worried about the looming clouds in the distance, how far away is that storm exactly? Add lightning detection with the AS3935 to your next weather station or your next bike ride!