MicroMod Asset Tracker Carrier Board Hookup Guide

≡ Pages
Contributors: El Duderino, PaulZC

Introduction

The MicroMod Asset Tracker Carrier Board provides you with a toolkit to monitor and track the location of your assets. Do you want to know where your assets are at all times? Or maybe you just want an update if an asset is moved? If so, this is the product for you!

SparkFun MicroMod Asset Tracker Carrier Board

DEV-17272
Retired

Built around the u-blox SARA-R510M8S module, the MicroMod Asset Tracker Carrier Board offers Secure Cloud LTE-M data communication for multi-regional use and has an integrated u-blox M8 GNSS receiver for accurate positioning information.

Want to be able to communicate directly with the SARA-R5 over USB-C, without needing a Processor Board? Or, want to upgrade the SARA firmware? The included Asset Tracker Update Tool lets you do just that. The Asset Tracker requires a Nano SIM for LTE-M connectivity. You can use the included Hologram eUICC SIM card or choose one from your preferred service provider if you prefer.

The Asset Tracker will work with any of our MicroMod Processor Boards, but because the asset tracker offers so many features and can be configured in different ways, some processor boards may be a better choice for your application than others. Please see “Choosing a Processor Board” below for more details.

The SARA-R5 supports many different forms of data communication from full TCP/IP sockets and packet switched data, through HTTP Get/Put/Post, FTP (the SARA has a built-in file system), Ping, to good old SMS text messaging!

The Asset Tracker has an integrated ICM-20948 Inertial Measurement Unit for 9-Degree Of Freedom orientation and movement detection. Want to send a message if your asset is moved? The asset tracker can do that! It also has a built-in digital microphone and so can send an alert as soon as a noise is detected too. Want to add a light sensor? The Qwiic connector will let you do that.

Want to use the Asset Tracker to log data during a journey or shipping? It has a built-in micro-SD card socket for data logging. Power options include both USB-C and LiPo battery (with built-in charging and battery fuel gauge), but you can provide power via a breakout pin too.

We’ve provided a full set of examples to get you up and running quickly and our SARA-R5 Arduino Library does all of the heavy lifting for you.

Required Materials

In addition to the MicroMod Asset Tracker Carrier Board, you’ll need a processor board to get started. Depending on which features of the SARA-R5 you want to use, some of our processor boards may be a better choice for your application. Please see “Choosing a Processor Board” below for more details.

SparkFun MicroMod nRF52840 Processor

WRL-16984
$29.50

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod SAMD51 Processor

DEV-16791
Retired

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

You'll also need a USB-C cable to connect the Carrier to your computer and if you want to add some Qwiic breakouts to your MicroMod project you'll want at least one Qwiic cable to connect it all together. Below are some options for both of those cables:

SparkFun Qwiic Cable Kit

KIT-15081
$12.95

Flexible Qwiic Cable - 100mm

PRT-17259
$1.95

Reversible USB A to C Cable - 2m

CAB-15424
$10.50

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

You can power the Asset Tracker via USB-C but for portable applications you'll need a single-cell LiPo battery too. Here are some examples:

Lithium Ion Battery - 2Ah

PRT-13855
$19.41

Lithium Ion Battery - 6Ah

PRT-13856
$48.44

Lithium Ion Battery - 1Ah

PRT-13813
Retired

You'll also need LTE and GNSS antennas. There are many to choose from, but here are some recommendations:

GNSS L1/L2 Multi-Band Magnetic Mount Antenna - 5m (SMA)

GPS-15192
$109.95

GPS/GNSS Magnetic Mount Antenna - 3m (SMA)

GPS-14986
$16.50

LTE Hinged External Antenna - 698MHz-2.7GHz, SMA Male

CEL-16432
Retired
Note: The SMA connections are standard polarity: the connector on the Asset Tracker is female, the antenna connection needs to be standard male. Antennas with reverse-polarity connectors are not suitable for the Asset Tracker.

Recommended Tools

You will need a screw driver to tighten the screw between the processor board and carrier board.

SparkFun Mini Screwdriver

TOL-09146
$1.50

Suggested Reading

If you are not familiar with the MicroMod ecosystem, we recommend reading here for an overview. We recommend reading here for an overview if you decide to take advantage of the Qwiic connector.

MicroMod Logo Qwiic Connect System
MicroMod EcosystemQwiic Connect System

Finally, if you aren't familiar with the following concepts you may want to check out a few of these tutorials before continuing.

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Hardware Overview

The MicroMod Asset Tracker has a lot going on so buckle up. In this section we'll cover the various components and hardware included on the Asset Tracker.

Common Components

Most SparkFun MicroMod Carriers will have some common components and all MicroMod Carriers will have the keyed M.2 MicroMod Connector to plug your processor into. The photo and list below outline some of the components you can expect on most SparkFun MicroMod Carriers.

  • M.2 MicroMod Connector - This special keyed M.2 connector lets you install your MicroMod Processor of choice on your Asset Tracker Carrier Board.
  • USB-C Connector - Connect to your computer to program your Processor and also can provide power to your MicroMod system.
  • 3.3V Regulator - Provides a regulated 3.3V and sources up to 1A.
  • Qwiic Connector - The standard Qwiic connector so you can add other Qwiic devices to your MicroMod system.
  • Boot/Reset Buttons - Push buttons to enter Boot Mode on Processor boards and to Reset your MicroMod circuit.
  • microSD Slot - Insert a microSD card for reading and writing data.
  • RTC Battery - We've included a 3V Lithium Rechargeable Battery as a backup power source for the Processor Board Real Time Clock (if present).

Annotated photo of common components.

u-blox SARA-R510M8S

The heart of the Asset Tracker is the SARA-R510M8S module from u-blox. This module does so much, it is difficult to know where to begin!

Photo highlighting SARA-R5 module, SMA connectors, SIM slot and SARA On button.

Note: The MicroMod Asset Tracker uses the "00B" product version of the SARA-R5 module (specifically the SARA-R510M8S-00B-00). LTE NB-IoT Radio Access Technology, and the LTE FDD bands: 66, 71, 85 are not supported by this version. Refer to the SARA-R5 datasheet for more information.

Designed to last an IoT lifetime, this module is 5G-ready with the u-blox UBX-R5 chipset. It has built-in end-to-end security with hardware-based root of trust inside a discrete secure element. It provides a full security suite with foundation, design and end-to-end security, as well as access control. The built-in u‑blox M8 GNSS receiver provides accurate and reliable positioning, always and everywhere. It is optimized for ultra-low power consumption and critical firmware updates can be delivered and services enabled via uFOTA (Firmware Over The Air). There. We told you it did a lot!

The SARA-R5 supports many different forms of data communication from full TCP/IP sockets and packet switched data, through HTTP Get/Put/Post, FTP (the SARA has a built-in file system), Ping, to good old SMS text messaging! The built-in GNSS receiver provides NMEA format data and our library looks after the parsing for you.

The connection between the SARA-R5 and the MicroMod Processor Board is serial (3.3V UART) but again, with this module being so clever, it can communicate over two serial interfaces at the same time. Want your LTE data on one interface and your GNSS data on a separate interface? It can do that too!

Note: Only some of our MicroMod Processors fuly support dual serial interfaces. If this is an important feature for you please see the "Choosing a Processor Board" section below for more details.

LTE and GNSS connections are via separate, robust SMA connectors. Switchable 3.3V power for an active antenna is available on the GNSS connector. The Asset Tracker includes a socket for a Nano SIM.

If you need to, you can manually turn the SARA off by pushing and holding the SARA On button. The SARA will disconnect from the network before going into low power sleep. Press the button briefly to turn the SARA back on again.

ICM-20948 IMU

The Asset Tracker carries the same ICM-20948 9-Degree Of Freedom Inertial Measurement Unit as OpenLog Artemis. It can provide fast accelerometer, gyro and magnetometer data and can be configured for “Wake On Motion” too. We have a WOM example ready to go. It has a built-in temperature sensor too.

Photo highlighting the ICM-20948 IMU.

Digital Microphone

Thieves are wily these days. When attempting to steal your asset, one of the first things they will do is cover or break the antenna (if they can see it). The built-in SPH0641 digital microphone can be used to send an alert as soon as the Asset Tracker hears the thieves coming!

Photo highlighting the digital microphone.

Battery Charging and Monitoring Circuit

Since many applications for the Asset Tracker involve a battery-powered circuit, the board includes both the MCP73831 LiPo battery charger and the MAX17048 battery fuel gauge. The MCP7381 Single-cell charge management IC can deliver a charge current up to 500mA. The MAX17048 is a low-power I2C fuel gauge to monitor your battery's remaining charge.

Photo highlighting the LiPo connector, charger and fuel gauge.

Plated Through-Hole (PTH) Connections

GPIO PTHs

We've broken out dedicated PTHs for digital, analog, pulse width modulation (PWM), I2C and SPI along the sides of the Asset Tracker Carrier Board. You may also notice that we've included a ground rail next to the digital, analog and PWM pins.

Photo highlighting the GPIO PTH header.

Power PTHs

We've also provided PTHs for monitoring and accessing the following power circuits:

  • VIN - The power rail fed by USB-C and/or the LiPo battery.
  • 3.3V - The regulated 3.3V rail which feeds most of the components on the board. You can measure the 3.3V current draw using the MEAS pins (see below).
  • VCCIO - This is the 1.8V rail generated by the SARA-R5. We use it to power the 1.8V to 3.3V level shifters for the UART and I2C connections.
  • 1.8V - This is the 1.8V rail which powers the IMU. You can disable it by pulling the MicroMod G4 digital pin LOW.
  • RST - Pull this low to reset the MicroMod Processor and the SARA-R5.

Photo highlighting the power PTH header.

SARA-R5 PTHs

The following SARA-R5 I/O connections are also broken out to PTH headers:

  • NI - This is the SARA's Network Indicator signal. It will be low (0V) when the network is available, and high (3.3V) when the network is not available.
  • TP - This is the Timing Pulse (1PPS) signal and is connected to SARA GPIO6/TP. It will pulse low and high when the SARA is receiving a GNSS signal and the timing pulse has been enabled. Please see Example11 for more details.
  • SARA USB D-/D+/DET - These PTHs provide access to the SARA's diagnostic USB port. This connection is only used to access the SARA's trace log. You cannot (currently) upgrade the SARA via this interface. Please consult the SARA R5 Integration Manual for more details.
  • SARA I2C - These 3.3V (level-shifted) PTHs can be used to access the SARA's I2C bus. Some models of the SARA-R5 use I2C to communicate with an external GNSS module. As the SARA-R510M8S has GNSS built-in, it is unclear what you might want to use them for. But, we've been diligent and have broken them out anyway!

Photo highlighting the SARA-R5 PTH pins.

SWD Programming Pins

An unpopulated JTAG footprint is available for more advanced users who need breakpoint level debugging. Note that this is not populated so you will need a compatible header and compatible JTAG programmer to connect.

Photo highlighting the JTAG footprint.

Solder Jumpers

If you have never worked with solder jumpers and PCB traces before or would like a quick refresher, check out our How to Work with Solder Jumpers and PCB Traces tutorial for detailed instructions and tips.

On the rear of the board, you will find a large number of jumpers which you can use to connect and disconnect several of the connections between the SARA and the MicroMod Processor:

Photo highlighting the solder jumpers on the Asset Tracker

Having trouble seeing the detail in the photo? Click on it for a larger view.


The tables below outline all of the jumpers on the Asset Tracker along with brief descriptions of their functionality.

Jumper Name/Label Description Default State Notes
G0 / SD CS Ties the µSD Chip Enable to G0 CLOSED
G1 / SD PWR Toggles 3.3V to control power the µSD card. CLOSED Open to isolate G1. µSD will default to always on.
G2 / LTE_PWR Connects G2 to the SARA-R5 ON signal via a level-shifting circuit. CLOSED Allows G2 to function in the exact same way as the SARA On button. Cut the jumper to isolate G2 if required.
G3 / IMU PWR When closed, G3 can be used to control power for the IMU via software. By default, IMU power is always on. OPEN On the ESP32 Processor G3 is linked directly to the processor's TX1 pin. Leave the G3 jumper OPEN if you are using the ESP32 Processor or else serial communication with the SARA will not work.
G4 / RI When closed, connects G4 to the SARA-R5's Ring Indicator pin. OPEN On the ESP32 Processor, G4 is shared with the processor's RX1 pin. Similarly, G4 is shared with SPI CIPO on the RP2040 Processor. Leave this jumper OPEN if using either Processor to avoid serial communication errors with the SARA.
G5 / SARA INT When closed, connects G5 with either the SARA-R5's Interrupt I/O pin or the SARA's GPIO3 I/O pin depending on the state of the EXT INT / GPIO3 dual jumper (covered below). OPEN On the RP2040 Processor, G5 is shared with SPI Chip Select line. Closing the jumper will interfere with the SPI bus on the RP2040 Processor.
G6 / SARA ON When closed, this jumper allows G6 to monitor if the SARA power is on. OPEN This signal is different to the SARA On push-button. On the RP2040 Processor, G6 is shared with the SPI Clock line. Closing this jumper will interfere with the SPI bus on the RP2040 Processor.
G7 / DSR When closed, connects G7 to the SARA's DSR signal. OPEN On the RP2040 Processor, G7 is shared with the SPI COPI line. Leave this jumper open to avoid interfering with the SPI bus on this processor.
PDM DAT Connects the data signal from on-board microphone to AUD_LRCLK (MicroMod Pad 52). CLOSED On the RP2040 Processor, AUD_LRCLK is shared with CTS1. Open this jumper to use the CTS connection on the SARA.
PDM CLK Connects the clock signal from the on-board microphone to AUD_BCLK (MicroMod Pad 50). CLOSED On the RP2040 Processor, AUD_BCLK is shared with RTS1. Open this jumper to use the RTS connection on the SARA.
I2C A dual jumper that ties SDA & SCL on the primary I2C/Qwiic bus to 3.3V via a pair of 2.2kΩ resistors. CLOSED Open both jumpers to disconnect the pull-ups.
SARA I2C A dual jumper that ties the SARA's SDA and SCL lines to 3.3V via a pair of 2.2kΩ CLOSED Open both jumpers to disable the pull-ups.
CIPO Ties SPI CIPO/SDI to 3.3V via a 2.2kΩ resistor. CLOSED Open to disconnect the pull-up. Opening this jumper may be advantageous for very low power applications where Processors like the Artemis have internal pull-ups which can be used instead.
EXT INT / GPIO3 A dual jumper used to select which signal is connected to MicroMod G5. SEE NOTE By default, this jumper is set so if the G5 / SARA INT jumper is closed, G5 is connected to the SARA EXT INT I/O pin. Switch this jumper to the opposite side to connect G5 to the SARA GPIO3 pin.
DSR A dual jumper used to control the direction of DSR from input to output . SEE NOTE By default, this jumper sets DSR as an input. Switching it sets DSR as an output so users can use dual-UART communication modes on the SARA.
MEAS Allows users to measure the current draw from the 3.3V power rail. CLOSED Open this jumper and complete the circuit using a digital multimeter to measure current draw on the 3.3V power rail.
VIN/3 Completes the VIN/3 voltage divider circuit. CLOSED Open the jumper to disable the VIN/3 voltage divider circuit. Disabling this can be useful in very low power applications to reduce total current draw.
3V3 (LED) Connects the anode of the 3.3V LED to 3.3V via a 1kΩ resistor. CLOSED Open the jumper to disable the 3.3V LED to reduce total current draw of the MicroMod circuit.
VIN (LED) Connects the anode of the VIN LED to VIN (5V if powered by USB, 3.7V nominal if powered by LiPo battery) via a 4.7kΩ resistor. CLOSED Open the jumper to disable the VIN LED to reduce the total current draw of the MicroMod circuit.
ICM_INT Connects the ICM IMU Interrupt pin to the primary I2C Interrupt pin (I2C_INT) on the MicroMod connector. CLOSED Open the jumper to isolate the MicroMod I2C_INT pin from the ICM-20948. On the RP2040 Processor, I2C_INT is shared with TX2. You may need to open this jumper to use the DTR handshake signal.
Jumper Name/Label Description Default State Notes
V USB Connects VUSB_DET on the SARA's diganostic (trace log) USB port to V_USB (5V OPEN Important! You must not have a Processor installed to use the diagnostic USB port.
USB D+ Connects USB_D+ on the SARA's diagnostic (trace log) USB port to USB_D+ on the USB-C connector. OPEN Important! You must not have a Processor installed to use the diagnostic USB port.
USB_D- Connects USB_D- on the SARA's diagnostic (trace log) USB port to USB_D- on the USB-C connector. OPEN Important! You must not have a Processor installed to use the diagnostic USB port.
VE When closed, allows the Processor to disable the main 3.3V regulator via the 3.3V_EN pin. OPEN Recommended only for very low power applications. The Processor can draw power from the RTC battery while the voltage regulator is disabled.
BYP Bypasses the 6V/2A fuse and nets VIN and V_USB together. OPEN The "penny-in-the-fuse" jumper. Close only if you know what you are doing!

MicroMod Pinout

Wondering what the pins are that are broken out on the MicroMod Asset Tracker Carrier Board? The tables below outline the Asset Tracker pinout as well as the general MicroMod pinout. Remember to compare the pins against your Processor Board to determine which pins are available.

Note: You may not recognize the COPI/CIPO labels for SPI pins. SparkFun is working to move away from using MISO/MOSI to describe signals between the controller and the peripheral. Check out this page for more on our reasoning behind this change.
AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
M.2 Connector Pin# MicroMod Pin Name Asset Tracker Connection Description
1 GND GND Ground plane.
2 3.3V 3.3V Regulated 3.3V via USB-C.
3 USB_D+ Passthrough USB D+ connection for Processor Board.
4 3.3V_EN 3.3V Enable Voltage regulator enable input.
5 USB_D- Passthrough USB D- connection for Processor Board.
6 RESET RESET Button Connected to RESET Button. Reset is active LOW
9 USB_VIN VIN Input voltage from USB.
10 D0 SPI PTH CS/D0 PTH SPI Chip Select for SPI PTH Header. D0 also broken out for I/O PTHs
11 BOOT BOOT Button Connected to BOOT Button. Boot is active LOW.
12 I2C_SDA I2C_SDA I2C data for Fuel Gauge & Qwiic connector
13 UART_RTS1 SARA RTS_I UART Request to Send for SARA
14 I2C_SCL I2C_SCL I2C clock for Fuel Gauge & Qwiic connector
15 UART_CTS1 SARA CTS_O UART Clear to Send for SARA
16 I2C_INT# IMU INT IMU Interrupt pin
17 UART_RX1 SARA TXD_O SARA UART Data Iutput
18 D1 D1 General digital I/O PTH
19 UART_TX1 SARA TXD_I SARA UART Data Output
20 UART_RX2 SARA DCD_O/RXD2_O SARA UART Data Carrier Detect / AUX UART Data Output
21 SWDCK SWDCK Serial Wire Debug Clock
22 UART_TX2 SARA DTR_I/TXD2_I SARA UART Data Terminal Ready / AUX UART Data Input
23 SWDIO SWDIO Serial Wire Debug I/O
32 PWM0 PWM0 PWM0 PTH
34 A0 A0 A0 PTH (Input Only)
34 A1 A1 A1 PTH (Input Only)
40 G0/BUS0 SD CS General purpose pin configured for Chip Select on µSD.
42 G1/BUS1 microSD_PWR General purpose pin configured for µSD Power Enable
44 G2/BUS2 LTE_PWR_ON General purpose pin configured for turning SARA on/off
46 G3/BUS3 ICM_PWR General purpose pin configured for controlling IMU power
48 G4/BUS4 SARA RI_O/CTS2_O SARA UART Ring Indicator / AUX UART Clear to Send
49 BATT_VIN/3 VIN/3 Divided input voltage for monitoring power supply.
50 AUD_BCLK I2S_SCK/PDM_CLK Microphone PDM clock signal
51 I2C_SDA1 SARA I2C SDA SARA I2C data signal
52 AUD_LRCLK I2S_WS/PDM_DAT Microphone PDM data signal
53 I2C_SCL1 SARA I2C SCL SARA I2C clock signal
55 SPI_CS# ICM_CS Chip select for IMU level shifting IC
57 SPI_SCK SPI_SCK SPI Clock
59 SPI_COPI SPI_SDO SPI controller out/peripheral in
61 SPI_CIPO SPI_SDO SPI controller in/peripheral out
69 G7/BUS7 SARA DSR_O/RTS2_I SARA UART Data Set Ready / AUX UART Request to Send
71 G6/BUS6 SARA_ON General purpose pin conifgured to monitor power for SARA
72 RTC_3V RTC_3V 3V output for backup battery charging.
73 G5/BUS5 SARA_INT General purpose pin configured for SARA Interrupt I/O pin
74 3.3V 3.3V 3.3V output from voltage regulator
Function Bottom
Pin
   Top   
Pin
Function
(Not Connected) 75 GND
3.3V 74 73 G5 / BUS5
RTC_3V_BATT 72 71 G6 / BUS6
SPI_CS1# SDIO_DATA3 (I/O) 70 69 G7 / BUS7
SDIO_DATA2 (I/O) 68 67 G8
SDIO_DATA1 (I/O) 66 65 G9 ADC_D- CAM_HSYNC
SPI_CIPO1 SDIO_DATA0 (I/O) 64 63 G10 ADC_D+ CAM_VSYNC
SPI COPI1 SDIO_CMD (I/O) 62 61 SPI_CIPO (I)
SPI SCK1 SDIO_SCK (O) 60 59 SPI_COPI (O) LED_DAT
AUD_MCLK (O) 58 57 SPI_SCK (O) LED_CLK
CAM_MCLK PCM_OUT I2S_OUT AUD_OUT 56 55 SPI_CS#
CAM_PCLK PCM_IN I2S_IN AUD_IN 54 53 I2C_SCL1 (I/O)
PDM_DATA PCM_SYNC I2S_WS AUD_LRCLK 52 51 I2C_SDA1 (I/O)
PDM_CLK PCM_CLK I2S_SCK AUD_BCLK 50 49 BATT_VIN / 3 (I - ADC) (0 to 3.3V)
G4 / BUS4 48 47 PWM1
G3 / BUS3 46 45 GND
G2 / BUS2 44 43 CAN_TX
G1 / BUS1 42 41 CAN_RX
G0 / BUS0 40 39 GND
A1 38 37 USBHOST_D-
GND 36 35 USBHOST_D+
A0 34 33 GND
PWM0 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 SWDIO
UART_TX2 (O) 22 21 SWDCK
UART_RX2 (I) 20 19 UART_RX1 (I)
CAM_TRIG D1 18 17 UART_TX1 (0)
I2C_INT# 16 15 UART_CTS1 (I)
I2C_SCL (I/0) 14 13 UART_RTS1 (O)
I2C_SDA (I/0) 12 11 BOOT (I - Open Drain)
D0 10 9 USB_VIN
SWO G11 8 7 GND
RESET# (I - Open Drain) 6 5 USB_D-
3.3V_EN 4 3 USB_D+
3.3V 2 1 GND
Signal Group Signal I/O Description Voltage
Power 3.3V I 3.3V Source 3.3V
GND Return current path 0V
USB_VIN I USB VIN compliant to USB 2.0 specification. Connect to pins on processor board that require 5V for USB functionality 4.8-5.2V
RTC_3V_BATT I 3V provided by external coin cell or mini battery. Max draw=100μA. Connect to pins maintaining an RTC during power loss. Can be left NC. 3V
3.3V_EN O Controls the carrier board's main voltage regulator. Voltage above 1V will enable 3.3V power path. 3.3V
BATT_VIN/3 I Carrier board raw voltage over 3. 1/3 resistor divider is implemented on carrier board. Amplify the analog signal as needed for full 0-3.3V range 3.3V
Reset Reset I Input to processor. Open drain with pullup on processor board. Pulling low resets processor. 3.3V
Boot I Input to processor. Open drain with pullup on processor board. Pulling low puts processor into special boot mode. Can be left NC. 3.3V
USB USB_D± I/O USB Data ±. Differential serial data interface compliant to USB 2.0 specification. If UART is required for programming, USB± must be routed to a USB-to-serial conversion IC on the processor board.
USB Host USBHOST_D± I/O For processors that support USB Host Mode. USB Data±. Differential serial data interface compliant to USB 2.0 specification. Can be left NC.
CAN CAN_RX I CAN Bus receive data. 3.3V
CAN_TX O CAN Bus transmit data. 3.3V
UART UART_RX1 I UART receive data. 3.3V
UART_TX1 O UART transmit data. 3.3V
UART_RTS1 O UART request to send. 3.3V
UART_CTS1 I UART clear to send. 3.3V
UART_RX2 I 2nd UART receive data. 3.3V
UART_TX2 O 2nd UART transmit data. 3.3V
I2C I2C_SCL I/O I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA I/O I2C data. Open drain with pullup on carrier board 3.3V
I2C_INT# I Interrupt notification from carrier board to processor. Open drain with pullup on carrier board. Active LOW 3.3V
I2C_SCL1 I/O 2nd I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA1 I/O 2nd I2C data. Open drain with pullup on carrier board. 3.3V
SPI SPI_COPI O SPI Controller Output/Peripheral Input. 3.3V
SPI_CIPO I SPI Controller Input/Peripheral Output. 3.3V
SPI_SCK O SPI Clock. 3.3V
SPI_CS# O SPI Chip Select. Active LOW. Can be routed to GPIO if hardware CS is unused. 3.3V
SPI/SDIO SPI_SCK1/SDIO_CLK O 2nd SPI Clock. Secondary use is SDIO Clock. 3.3V
SPI_COPI1/SDIO_CMD I/O 2nd SPI Controller Output/Peripheral Input. Secondary use is SDIO command interface. 3.3V
SPI_CIPO1/SDIO_DATA0 I/O 2nd SPI Peripheral Input/Controller Output. Secondary use is SDIO data exchange bit 0. 3.3V
SDIO_DATA1 I/O SDIO data exchange bit 1. 3.3V
SDIO_DATA2 I/O SDIO data exchange bit 2. 3.3V
SPI_CS1/SDIO_DATA3 I/O 2nd SPI Chip Select. Secondary use is SDIO data exchange bit 3. 3.3V
Audio AUD_MCLK O Audio master clock. 3.3V
AUD_OUT/PCM_OUT/I2S_OUT/CAM_MCLK O Audio data output. PCM synchronous data output. I2S serial data out. Camera master clock. 3.3V
AUD_IN/PCM_IN/I2S_IN/CAM_PCLK I Audio data input. PCM syncrhonous data input. I2S serial data in. Camera periphperal clock. 3.3V
AUD_LRCLK/PCM_SYNC/I2S_WS/PDM_DATA I/O Audio left/right clock. PCM syncrhonous data SYNC. I2S word select. PDM data. 3.3V
AUD_BCLK/PCM_CLK/I2S_CLK/PDM_CLK O Audio bit clock. PCM clock. I2S continuous serial clock. PDM clock. 3.3V
SWD SWDIO I/O Serial Wire Debug I/O. Connect if processor board supports SWD. Can be left NC. 3.3V
SWDCK I Serial Wire Debug clock. Connect if processor board supports SWD. Can be left NC. 3.3V
ADC A0 I Analog to digital converter 0. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
A1 I Analog to digital converter 1. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
PWM PWM0 O Pulse width modulated output 0. 3.3V
PWM1 O Pulse width modulated output 1. 3.3V
Digital D0 I/O General digital input/output pin. 3.3V
D1/CAM_TRIG I/O General digital input/output pin. Camera trigger. 3.3V
General/Bus G0/BUS0 I/O General purpose pins. Any unused processor pins should be assigned to Gx with ADC + PWM capable pins given priority (0, 1, 2, etc.) positions. The intent is to guarantee PWM, ADC and Digital Pin functionality on respective ADC/PWM/Digital pins. Gx pins do not guarantee ADC/PWM function. Alternative use is pins can support a fast read/write 8-bit or 4-bit wide bus. 3.3V
G1/BUS1 I/O 3.3V
G2/BUS2 I/O 3.3V
G3/BUS3 I/O 3.3V
G4/BUS4 I/O 3.3V
G5/BUS5 I/O 3.3V
G6/BUS6 I/O 3.3V
G7/BUS7 I/O 3.3V
G8 I/O General purpose pin 3.3V
G9/ADC_D-/CAM_HSYNC I/O Differential ADC input if available. Camera horizontal sync. 3.3V
G10/ADC_D+/CAM_VSYNC I/O Differential ADC input if available. Camera vertical sync. 3.3V
G11/SWO I/O General purpose pin. Serial Wire Output 3.3V

Board Dimensions

The Asset Tracker Carrier Board measures 3.0 inches by 3.0 inches (76.2mm x 76.2mm) and has four mounting holes that fit a 4-40 screw.

Asset Tracker Board Dimensions

Having trouble seeing the details in the image? Click on it for a larger view!

Choosing a Processor Board

As you can see from the Jumpers section above, there are some things to consider when choosing a MicroMod Processor Board to go with your Asset Tracker.

The MicroMod M.2 connector pinout is very comprehensive and some of the processor chips on our MicroMod Processor Boards just don't have enough I/O pins to let us allocate one to every M.2 pin. So, on those boards we share the pins. For example, on the ESP32 Processor Board, you will see that the UART TX1 pin is shared with the G3 I/O pin and the AUD_OUT pin. We do that so that you can use that pin for TX1 or G3 or AUD_OUT. And for most users and most Carrier Boards, that's perfectly fine. However, since the SARA-R5 has so many pins that we need to connect to, the sharing of TX1 and G3 causes a small problem. We need TX1 to communicate with the SARA, and G3 would normally be used to enable power for the ICM-20948 IMU. We get round that by including a normally-open split pad jumper on G3 and making the IMU power circuit default to on. Simple!

So, you can use any SparkFun MicroMod Processor in the Asset Tracker, but if you need complete access to all of the pins then here are the restrictions:

ESP32 Processor

TX1 is shared with G3. This means you cannot close the G3 split pad to enable control of the IMU Power. The IMU power will need to be always on.

RX1 is shared with G4. This means you cannot close the G4 split pad to access the SARA Ring Indicator / Clear To Send 2 pin.

AUD_LRCLK is shared with G1. G1 controls the micro-SD power and AUD_LRCLK is connected to the digital microphone. If you want to use the microphone, you will need to open the G1 split pad jumper. The micro-SD power will default to on.

AUD_BCLK is shared with G2. G2 can be used to turn the SARA-R5 on/off and AUD_BCLK is connected to the digital microphone. If you want to use the microphone, you will need to open the G2 jumper. You won’t then be able to have the processor turn the SARA on and off. The SARA always powers on automatically when power is connected, so no worries there, and the SARA On button is there if you need it.

Artemis Processor

The Artemis Processor does not support the M.2 TX2 and RX2 pins. This means you cannot use the Artemis to talk to the SARA using any of the dual-UART variants (called variants 2, 3 and 4 in the SARA-R5 System Integration Manual). This means you cannot, for example, use UART 1 for your LTE traffic and UART 2 for your GNSS data. That's all. You can do everything over a single UART anyway.

nRF5280 Processor

The nRF52840 Processor Board supports all of the pins used by the Asset Tracker. There are no restrictions for this Processor Board.

SAMD51 Processor

The SAMD51 Processor Board does not support RTS1 and CTS1 and so you will not be able to perform hardware handshaking when using the UART. Serial buffers are so large these days that you probably won’t even notice this restriction, but it is something to be aware of.

RP2040 Processor

AUD_LRCLK is shared with CTS1. This means that if you want to use hardware handshaking for the UART communication, you won’t be able to use the digital microphone.

Likewise AUD_BCLK is shared with RTS1, again preventing you from using the microphone and hardware handshaking at the same time.

I2C_INT is shared with TX2. This means that you cannot use the ICM-20948 IMU interrupt and SARA DTR / TXD2 simultaneously. You can open the ICM_INT split pad to isolate the IMU interrupt signal.

G4, G5, G6 and G7 are shared with the SPI connections SPI_SCK, SPI_COPI, SPI_CIPO and SPI_CS. This should not be an issue for you, but it does mean you cannot close the G4-G7 jumpers to enable access to: SARA_RI, SARA_INT, SARA is On, and SARA_DSR.

STM32 Processor

The STM32 Processor Board does not support RTS1 and CTS1 and so you will not be able to perform hardware handshaking when using the UART. Serial buffers are so large these days that you probably won’t even notice this restriction, but it is something to be aware of.

The STM32 Processor Board does not support the M.2 TX2 and RX2 pins. This means you cannot use the STM32 to talk to the SARA using any of the dual-UART variants (called variants 2, 3 and 4 in the SARA-R5 System Integration Manual). You cannot, for example, use UART 1 for your LTE traffic and UART 2 for your GNSS data.

G7 is not supported on the STM32 Processor Board. This should not be an issue for you, but it does mean you cannot access the SARA is On signal.

Hardware Assembly

Now that we are familiar with the hardware on the Asset Tracker Carrier Board, it's time to assemble it with your chosen MicroMod Processor and get it connected to your computer.

Inserting Your Processor

With the M.2 MicroMod connector, connecting your processor board is a breeze. Simply match up the key on your processor's beveled edge connector to the key on the M.2 connector. At a 45° angle, insert the processor board to the M.2 connector. The processor board will stick up at an angle as seen here:

Photo showing the Processor inserted into M.2 connector at 45 degree angle.

Once the board is in the socket, gently press the Processor down, grab the set screw and tighten it with a Phillip's head screwdriver:

Photo showing the Processor being secured with a screwdriver.

With the Processor secure, your assembled MicroMod Asset Tracker system should look similar to the image below!

Photo showing a properly secured Processor Board.

Note There is technically no way to insert the Processor backwards since the key prevents from mating with the M.2 connector. As an extra safeguard to prevent inserting a Processor improperly or with a poor connection, the mounting screw will not match up if the Processor is not plugged in entirely.

Connecting Everything Up

Now is a good time to insert the Nano SIM from your service provider. Make sure the orientation matches the symbol on the PCB; the edge with the trimmed corner is inserted first.

The LTE and GNSS connections simply screw on to the appropriate SMA connectors. Make sure you check the labeling on the board and connect them the right way round. (LTE is on the Left.)

MicroMod Asset Tracker fully assembled circuit with antennas

With your processor inserted and secured it's time to connect your MicroMod Asset Tracker Carrier Board to your computer using the USB-C connector. Depending on which processor you choose and which drivers you already have installed, you may need to install drivers for your board. Refer to your Processor's Hookup Guide for detailed instructions on how to install them.

Software Setup

Note: The software examples assume you are using the latest version of the Arduino IDE on your computer. If this is your first time using Arduino, please review our tutorial on Installing the Arduino IDE. If you have not previously installed an Arduino library, please read through our Arduino Library Installation Guide
Note: Make sure that for whichever MicroMod Processor you choose, you have the correct board definitions installed.

The Asset Tracker examples will run on any SparkFun MicroMod Processor Board (PB) but each PB has a slightly different sequence to follow when uploading and running code. For example, some require a press of the Boot button and others do not. Head over to our MicroMod Processor Boards landing page, find your Processor, and read through its tutorial for help installing your board definition and how to upload the code.

We have prepared a complete set of examples showing you how to use all of the features on the Asset Tracker. However, the examples need access to several Arduino Libraries before they will run correctly and so you need to install those too.

Installing the MicroMod Asset Tracker Carrier Board Examples

The Asset Tracker examples live on GitHub in the Asset Tracker repository and you will find them in the Examples folder. You can download the complete repository from GitHub as a single .ZIP file by clicking the button below:

Unzip the .ZIP file and copy all 22 examples to a suitable folder on your computer. We recommend putting them in your Arduino folder.

You will see that each example comprises three files. E.g for Example1:

  • AssetTracker_Example1_Blink.ino is the actual example code
  • AssetTrackerPins.h contains the pin definitions to allow each Processor to work correctly with the Asset Tracker
  • AssetTrackerPins.ino contains useful ‘housekeeping’ functions that do things like turn on the SD or IMU power. They are in a separate file to make them easier to update when we add new processor boards and to avoid cluttering up the main example code.

When it is time to open and try Example1 select the AssetTracker_Example1_Blink.ino file first. The other two will open automatically as they are in the same folder.

SparkFun u-blox SARA-R5 Arduino Library

The SparkFun u-blox SARA-R5 Arduino Library lives on GitHub too and you can either install it using the Arduino Library Manager, or you can install it manually.

If you want to install the library using the Arduino Library Manager, then search for ‘SparkFun u-blox SARA-R5’.

Alternatively, you can download a .ZIP of the library by clicking the button below:

Additional Libraries

Once you have the u-blox SARA-R5 library installed, most (but not all) of the examples will work correctly. To allow the full set to run, you also need to install the following libraries:

You can install them using the Arduino Library manager by searching for their respective names. Alternatively, you can download the .ZIP for each of them by clicking the buttons below:

Arduino Examples

Once you have the MicroMod Asset Tracker Carrier Board examples and all of the required libraries installed, it is finally time to run your first example!

Example 1: Blink

Baby steps… Example1 checks that you can communicate with the MicroMod Processor Board, compile and upload code successfully.

Navigate to the location the Asset Tracker Examples repository downloaded to and open the Examples folder. In that folder you'll find all the examples. Navigate to Example1 and open the file called AssetTracker_Example1_Blink.ino in the Arduino IDE or copy the code below into a blank sketch, select your Board and Port and click "Upload".

language:c
#include "AssetTrackerPins.h" // Include the Asset Tracker pin and port definitions

#define SERIAL_PORT Serial // This is the console serial port - change this if required

#include <SparkFun_u-blox_SARA-R5_Arduino_Library.h> //Click here to get the library: http://librarymanager/All#SparkFun_u-blox_SARA-R5_Arduino_Library

// Create a SARA_R5 object to use throughout the sketch. Pass it the power pin number.
SARA_R5 assetTracker(SARA_PWR);

void setup()
{
  initializeAssetTrackerPins(); // Initialize the pins and ports (defined in AssetTrackerPins.ino)
}

void loop()
{
  digitalWrite(LED_BUILTIN, !digitalRead(LED_BUILTIN)); // Flash the STAT LED at 0.5Hz (Read-Invert-Write)
  delay(1000);
}

All Example1 does is blink the STAT LED on the Processor Board. That's all it does. Yes, really. But it proves that you have the correct Processor Board selected and that code compilation and upload works. The good stuff comes in the following examples.

Example 2: IMU

Example2 demonstrates how to get readings from the ICM-20948 Inertial Measurement Unit on the Asset Tracker. Open AssetTracker_Example2_IMU.ino and upload to the Processor Board. Now open the Serial Monitor or a terminal emulator and connect to the Processor Board at 115200 Baud. If all is well, you should see the following:

Screenshot showing Arduino Serial Monitor open

Click Send or hit Enter and you should then see the following, followed by lots of lovely IMU data scrolling up the screen:

Screenshot of Arduino Serial Monitor printing IMU data.

The things to look out for are a 980 milli-g Acceleration in Z - if your board is horizontal. That's gravity. You will also see a reading of the Earth's magnetic field on one or more of the Magnetometer (Compass) axes, but the value will depend on your local Angle Of Magnetic Declination and Inclination. (Strange but true: the strongest magnetic field points downward into the ground in many places.)

Example 3: µSD Card

Example3 uses Bill Greiman's SdFat library to print a directory of all the files on your microSD card.

The usual restrictions apply: we recommend disconnecting the power to your Asset Tracker before removing or inserting the µSD card. Removing the card while powered can cause data corruption.

Example 4: MAX17048 Fuel Gauge

Example4 demonstrates how to use the MAX17048 Fuel Gauge to read the battery charge status.

Example 5: Qwiic

Example5 demonstrates how to use the Qwiic bus to talk to an external sensor attached to the Qwiic connector. The example assumes that you have a Qwiic Power Switch attached, but you can adapt the code to use whichever Qwiic board you have available. The Qwiic I2C bus is called Wire on the Asset Tracker.

Example 6: I/O Pins

Example6 demonstrates how to configure the D0, D1, A0, A1, PWM0 and PWM1 Input / Output pins.

Example 7: GNSS Antenna Power

Example7 is where we communicate with the SARA-R5 for the first time. The power for the active GNSS antenna is controlled by the SARA GPIO2 pin. When the SARA is on and GPIO2 is high, the 3.3V antenna power is enabled. We need to instruct the SARA to enable GPIO2 and set it high via the UART interface.

The example code calls enableGNSSAntennaPower(); and disableGNSSAntennaPower(); which do the heavy lifting for you. Those functions are defined in AssetTrackerPins.in and in turn call the SARA-R5 library:

language:c
assetTracker.setGpioMode(assetTracker.GPIO2, assetTracker.GPIO_OUTPUT, 1); // Enable

and

language:c
assetTracker.setGpioMode(assetTracker.GPIO2, assetTracker.GPIO_OUTPUT, 0); // Disable

There is no indicator LED to tell you if the antenna power is on. You can, if you wish, use a digital multimeter to probe carefully on the center pin of the GNSS SMA connector. You will see voltage toggling between 3.3V and 0V.

Important! When probing the GNSS SMA connector be very careful to avoid static discharge. A grounding strap is recommended to prevent damaging the antenna and board from static discharge.

This example demonstrates that serial communication is taking place between the Processor Board and the SARA-R5.

Example 8: External SPI

Example8 shows how to use the SPI Breakout Plated-Through Holes (PTHs) on the left edge of the board. The example assumes you have a SparkFun Micro OLED Display connected, but you can adapt the code to talk to whichever SPI board you have available. The SPI port is called SPI on the Asset Tracker.

Example 9: VIN

Example9 demonstrates how to read the VIN bus voltage using the resistor divider on the Asset Tracker. The function readVIN() in AssetTrackerPins.ino automatically converts the Analog To Digital Converter result into voltage correctly for the different Processor Boards.

Example 10: IMU Wake-On-Motion

Example10 demonstrates how the ICM-20948 IMU can be configured to detect motion or an impact. This example could be a key part of your final asset-tracking code.

Example 11: GNSS GPRMC

Example11 demonstrates how to read the Asset Tracker’s location using the u-blox M8 GNSS receiver built into the SARA-R5. The GNSS generates an NMEA GPRMC data stream and our SARA-R5 library does the heavy lifting for you, extracting the latitude and longitude etc. as numbers.

Example 12: Identification

Example12 is the first example which communicates with the LTE part of SARA-R5. The example reads data from the SARA including its ID, firmware version, serial number, IMEI and subscriber number. The subscriber number - if present - comes from the SIM. This example demonstrates that the SIM is inserted correctly.

Example 13: Network Information

Example13 is the first example which checks that the SARA is receiving an LTE signal. The code prints the received signal strength, registration status and data “context ID”. The SARA reads your operator details from the SIM and uses those when registering on the network.

It is important that you run examples 13, 14 and 17 in order as each plays a role in making sure the SARA's data connection is configured correctly.

Example 14: Register Operator

Example14 shows if you are already connected to a network and gives you the opportunity to register on a different network (if one is available and if your SIM supports this). You can use this example to list all of the LTE operators the SARA can detect, but you will only be able to connect to networks supported by your SIM.

Example 15: Receive SMS

For many applications, good old Short Message Service text messaging is a good solution. Example15 demonstrates how to read and print any existing text messages in the SARA's memory. The code will then wait for a new message to arrive and will print it when it does.

Incoming messages are automatically marked as read once they have been printed by the code. You can force the code to print all the messages in memory by commenting the line which says:

language:c
if (unread == "REC UNREAD") // Only print new (previously-unread) messages.

Screenshot showing serial printout of SMS messages and message data

Example 16: Send SMS

Example16 demonstrates how to send an SMS message to another phone or Asset Tracker. The code will ask for the destination number, followed by the message. If you are using the Arduino IDE Serial Monitor, you can type these into the text box at the top of the window and then click Send or press Enter. If you are using a terminal emulator, type the number and then press Enter (or add a newline / line feed character (“\n” or 0x0A)) to end the message.

Example 17: Packet Switched Data

Example17 is an important example as it configures the “Context Identifier” for your mobile data connection. The SARA will read details of the data context from the network and SIM and you can confirm which one you want to use. The first context may be blank; select one that shows a sensible name and IP address for your service provider. In the screenshots below, we select option 1:

Screenshot showing serial monitor printout for Example 17

Screenshot showing serial monitor printout after entering "1" for Example 17

The code provides a warning that “deactivate profile failed”. We see this because the SARA needs to disconnect from a profile before it can connect to a new one, and in this case this failed because there was no profile active. Don’t worry about this warning, it is just there for information. The example shows that our connection was successful by displaying the Internet Protocol (IP) address the SARA has been allocated by the service operator.

Example 18: Ping

Example18 tests the SARA's data connection by performing one of the oldest and shortest data transfers going… A ping!

The code will ask for the name of the server you want to ping. www.google.com is a good choice, but www.sparkfun.com works too! If the ping is successful, you will see the time it took for the ping to do a round trip in milliseconds.

Screenshot showing serial printout from successful ping.
Having trouble seeing the detail in this image? Click on it for a larger view.

If the ping is not successful, one option to find out why is to uncomment the line which says:

language:c
assetTracker.enableDebugging(SERIAL_PORT); // Uncomment this line to enable helpful debug messages

This enables a bunch of helpful debug messages that print in the Serial Monitor or your terminal emulator window. After uncommenting the above line, upload the code again.

Look for any messages that include +UUPINGER:. That will give you the cause of the PING ERror. The SARA-R5 AT Command Reference contains the full list of Ping error codes in Appendix A.10.

For example, error 8 means that the SARA “Cannot resolve host” which is usually a sign that a Domain Name Server (DNS) is not available. Error 17 indicates “Packet Switched Data connection not established”. If you see errors like this, please make sure you ran examples 13, 14, 17 and 18 in order. Each builds on the previous example.

Example 19: ThingSpeak

Example19 demonstrates how to send data to ThingSpeak using HTTP POST or GET.

Prior to using this example you need to complete the following steps:

  • Create a ThingSpeak User Account here
  • Create a new Channel by selecting Channels --> My Channels --> New Channel
  • Note the Write API Key and copy/paste it into myWriteAPIKey in the example code.

The example code reads the temperature from the Asset Tracker IMU and POSTs it to ThingSpeak. It will be added to your ThingSpeak channel as "Field 1".

Note: The IMU temperature is always a few degrees warmer than ambient as it is inside a nice warm chip busy running accelerometer, gyro and compass sensors!

If you open your serial monitor at 115200 baud the code prints out over serial the data sent to ThingSpeak:

Screenshot showing serial monitor printout while temperature data is posted to ThingSpeak.

Check your ThingSpeak channel and you should see data posted to it similar to the screenshot below:

Screenshot of ThingSpeak application showing temperature data posts.

Examples 20-22: Production Tests

Examples 20 - 22 are the ones we use using Asset Tracker production tests to check if the SARA’s I/O pins are connected correctly. We’ve included them as you might find them useful if you want to control the pins on the SARA. The examples use the SARA’s +UTEST mode to control the pins. Please consult the SARA-R5 AT Command Reference for further details.

Troubleshooting

In this section we'll go over a few troubleshooting tips for common snags and questions using the MicroMod Asset Tracker Carrier Board.

LTE Network Availability

The SARA-R5 supports LTE-M and NB-IoT data communication for multi-regional use. Please check the LTE signal availability for your area before purchasing a SARA-R5 product and selecting an LTE service provider / operator.

Data Connectivity

When working through the data connectivity examples, it is important that you run examples 13, 14 and 17 in order, before moving on to example 18 or 19. Each example builds on the last and together they configure the SARA’s data connection correctly.

TP (1PPS) Pin and LED

At the time of writing, we are shipping the SARA-R5 on the Asset Tracker with firmware version 02.06 on it. 02.06 contains a feature (which is just a polite name for a bug!) which means the 1 Pulse-Per-Second from the GNSS does work, but the pulse is only ~3 microseconds wide and cannot be adjusted. Handy huh? u-blox are aware of this - in fact we told them about it - and a fix is coming but they haven’t added it yet. We will keep an eye out for it and update this section once the fix is released.

Just to complicate matters, 3 microseconds is too short for the buffer FET and LED connected to the timing pulse to respond. So, we regret that you cannot currently use the TP PTH. We will share the fix with you as soon as we have it. The SARA firmware is easy to update using the Asset Tracker Firmware Update Tool.

NB/IoT Compatibility

The SparkFun MicroMod Asset Tracker uses the "00B" product version of the SARA-R5 module (specifically the SARA-R510M8S-00B-00). LTE NB-IoT Radio Access Technology, and the LTE FDD bands: 66, 71, 85 are not supported by this version.

General Troubleshooting Help

Resources and Going Further

Now that you've successfully got your MicroMod Asset Tracker Carrier Board up and running with your Processor Board, it's time to incorporate it into your own tracking project! For more information, check out the resources below:

MicroMod Asset Tracker Carrier Documentation:

u-blox SARA-R5 LTE-M / NB-IoT module Documentation:

MicroMod Documentation:

Users looking to update the firmware on their Asset Tracker Carrier Board using the MicroMod Update Tool should read through our MicroMod Update Tool Hookup Guide:

MicroMod Update Tool Hookup Guide

February 25, 2021
Follow this guide to learn how to use the MicroMod Update Tool to interact directly with the UART on the MicroMod Asset Tracker's SARA-R5. Using this board you can talk directly to the module using u-blox's m-center software as well as update the firmware using EasyFlash.

Need some inspiration for your next project? Check out some of these related tutorials with MicroMod:

MicroMod Weather Carrier Board Hookup Guide

A quick guide to help to create your own MicroMod weather station using the MicroMod Weather Carrier Board and Processor of your choice.

MicroMod All The Pins (ATP) Carrier Board

Access All The Pins (ATP) of the MicroMod Processor Board with the Carrier Board!

MicroMod Main Board Hookup Guide

The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.

MicroMod STM32WB5MMG Hookup Guide

Add a powerful combination of computing power and wireless communication to your next MicroMod project with the SparkFun MicroMod STM32WB5MMG Processor.