MicroMod Artemis Processor Board Hookup Guide

≡ Pages
Contributors: Nate, Ell C

Example 1: Blink

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

To get started uploading code and working with your Machine Learning Carrier Board, make sure you have the Artemis MicroMod board definition selected under your Tools > Board menu (or whatever processor you've chosen to use).

Arduino Board Select

Having a hard time seeing? Click the image for a closer look.


Then select your serial port under the Tools > Port menu.

Port Selection for the Artemis MicroMod Processor Board

Loading Blink

Let's start with something basic - let's blink an LED. Go to File->Examples->01.Basics->Blink.

Blink Basics Example in the pulldown

Having a hard time seeing? Click the image for a closer look.


With everything setup correctly, upload the code! Once the code finishes transferring, you should see the STAT LED on the Artemis Processor Board begin to blink!

If the blue LED remains off, it's probably still sitting in the bootloader. After uploading a sketch, you may need to tap the reset button to get your Artemis MicroMod to run the sketch.

Look at all the blinks!

blink blink blink