MEMS Microphone Hookup Guide

≡ Pages
Contributors: jenfoxbot

Hardware Hookup (Quickstart)

If all of this is super familiar, here's all you need to get started:

  1. For a temporary connection, you can use IC hooks. For a permanent connection, we recommend soldering three wires (or headers) to each MEMS microphone breakout board ports.

  2. Connect the Vcc port to 3.3V (or anything between 1.5 and 3.3V) and the GND port to ground.

  3. Connect the AUD port to an analog (ADC) input on a microcontroller.

  4. Read in the ADMP401 analog signal and measure/record all the sounds! (Also remember it's a sound signal, so you'll likely want to use the amplitude of the sound wave rather than the raw voltage output.)

Wires Soldered to ADMP401 IC Hook Connected to ICS-40180
Wires Soldered to ADMP401 IC Hook Connected to ICS-40180