MEMS Microphone Hookup Guide

≡ Pages
Contributors: jenfoxbot

Hardware Hookup

For a more in-depth example, follow along with the following steps:

  1. For a temporary connection, you can use IC Hooks. For a permanent connection, solder three wires (or header pins) to the breakout board ports. We recommend using the following colors to easily distinguish the board ports. If you do not have the color wire available, you can always select a different color as well.

    • red for Vcc
    • black for GND
    • yellow (or some other color) for AUD

  2. Connect the Vcc port to the 3.3 V output of a microcontroller (or any power supply between 1.5 and 3.3 V).

  3. Connect the GND port to GND on the microcontroller.

  4. Connect the AUD port to an analog, or ADC, input on the microcontroller. In this case, we are using A0.

Wire Connected to Arduino IC Hooks Connected to Arduino

You can also use the following hookup table as a quick reference.

Arduino MEMS Microphone
A0 AUD
GND GND
3.3V VCC

The next section will cover how to read the audio signal from the microphone to a microcontroller.