LilyPad Basics: E-Sewing

≡ Pages
Contributors: Gella

Sewing with Conductive Thread

Most LilyPad projects use conductive thread to complete electrical circuits. The following sections will introduce you to some basic sewing techniques as well as a few special pointers for using conductive thread to build working circuits. Even if you’re already familiar with using a needle and thread, this section may still be useful to you, specifically where it pertains to sewing with LilyPad parts.

alt text

Securing Your Components

Each LilyPad piece has large holes with conductive silver pads called sew tabs. These tabs are designed to give you plenty of room to pass a needle and thread through the hole several times. Before you begin stitching your circuit, identify the sew tabs you would like to connect, and orient them so they are easily accessible in your design. If following along with SparkFun templates, the pieces will have a specific location on the design for both ease of sewing and visual appeal.

alt text

We recommend using a small dot of hot glue (preferred) or fabric glue to attach each LilyPad piece to the fabric to keep it from moving while you sew. Make sure not to accidentally seal up the holes in the sew tabs.

Glue LEDsPlace LEDs

To help plan where the stitches will go, you can use a marker to draw lines between the components.

Draw Lines

Threading a Needle

Cut a piece of conductive thread approximately 2 feet long. Push one end of the thread through the eye (opening) of the needle and pull through, leaving a tail of about 5 inches.

alt text

Before you begin sewing your project, you will need to tie a knot at the long end of the thread to prevent you from completely pulling it through the fabric. You can tie a simple overhand or square knot. The next sections will explain a few other knot methods.

Starter Knot

A starter knot is a method of starting your stitch with a knot directly on your fabric.

alt text

Quilter's Knot

The slightly more advanced quilter’s knot is a way to tie a quick, secure knot on the thread. After some practice, this knot can be tied very quickly.

alt text

Connecting To LilyPad Sew Tabs

We’ll stitch conductive thread around LilyPad sew tabs in our circuits to connect the pieces together. It’s important that you make three to four loops each time you connect your thread around an empty sew tab and pull the thread snug with each pass. This ensures you have made a strong electrical and physical connection between the thread and the sew tab. Pull loops tight before continuing your stitch.

alt text

Sewing Basics

After sewing loops around a sew tab, a running stitch will enable you to connect LilyPad pieces together with a continuous length of conductive thread. Follow these steps:

Push the needle through the fabric about 1/4" in the direction of your stitch path.

alt text

Pull the slack of the thread through so it sits flush with the fabric.

alt text

Push the needle back up through the fabric another 1/4" along the stitch path.

alt text

Pull the slack of the thread through so it sits flush with the fabric.

alt text

Repeat this process to travel along the path to the next LilyPad piece you want to connect to, keeping stitches evenly spaced.

alt text

Running vs. Hidden Stitch

In a basic running stitch, the stitching will be even on both sides of the fabric.

alt text

To hide the stitches so that they are not seen on the outside of the project, make a longer stitch on the back of the project and a very small stitch on the front of the project. This method is called a “hidden stitch.”

alt text

As you sew, flip your fabric over every so often to make sure the conductive thread isn’t getting knotted or tangled. If you are just starting out with sewing, your stitching may take some practice before it feels comfortable or easy. Remember to be patient with yourself and take your time while stitching. If your thread breaks, you can stitch onto existing conductive thread to continue the electrical connection.

Connecting LilyPad Pieces

Both running and hidden stitches will enable you to connect LilyPad components together with a single length of conductive thread. To connect two LilyPad pieces, continue stitching after completing three to four loops around the sew tab.

alt text

alt text

Connecting Multiple LilyPad Pieces

To connect more than two LilyPad pieces, instead of trimming your thread and starting over, continue stitching to the next piece, make three to four loops, and repeat as necessary. There is no need to use a new length of thread if the pieces will share a connection.

alt text

alt text

Finishing Your Connection

When you have completed connecting components, use a finishing knot. Thread tails can cause electrical shorts, so be sure to trim your thread afterward.

alt text