Large Digit Driver Hookup Guide

≡ Pages
Contributors: Shawn Hymel

Example: One Large Digit

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

If you have not previously installed an Arduino library, please check out our installation guide.

Load the Single Digit Example Code

Plug your Arduino into your computer via USB cable. Open up the Arduino program and copy in the following sketch.

language:c
    /*
 Controlling large 7-segment displays
 By: Nathan Seidle
 SparkFun Electronics
 Date: February 25th, 2015
 License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).

 The large 7 segment displays can be controlled easily with a TPIC6C594 IC. This code demonstrates how to control
 one display.

 Here's how to hook up the Arduino pins to the Large Digit Driver

 Arduino pin 6 -> CLK (Green on the 6-pin cable)
 5 -> LAT (Blue)
 7 -> SER on the IN side (Yellow)
 5V -> 5V (Orange)
 Power Arduino with 12V and connect to Vin -> 12V (Red)
 GND -> GND (Black)

 There are two connectors on the Large Digit Driver. 'IN' is the input side that should be connected to
 your microcontroller (the Arduino). 'OUT' is the output side that should be connected to the 'IN' of addtional
 digits.

 Each display will use about 150mA with all segments and decimal point on.
*/

//GPIO declarations
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
byte segmentClock = 6;
byte segmentLatch = 5;
byte segmentData = 7;

//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

void setup()
{
  Serial.begin(9600);
  Serial.println("Large Digit Driver Example");

  pinMode(segmentClock, OUTPUT);
  pinMode(segmentData, OUTPUT);
  pinMode(segmentLatch, OUTPUT);

  digitalWrite(segmentClock, LOW);
  digitalWrite(segmentData, LOW);
  digitalWrite(segmentLatch, LOW);

  int x = 0;
  while(1)
  {
    if(x == 9)
      postNumber(x, true); //Show decimal
    else
      postNumber(x, false);

    digitalWrite(segmentLatch, LOW);
    digitalWrite(segmentLatch, HIGH); //Register moves storage register on the rising edge of RCK
    delay(500);

    x++;
    x %= 10; //Reset x after 9

    Serial.println(x); //For debugging
  }
}

void loop()
{
  //showNumber(42); //Test pattern
}

//Takes a number and displays 2 numbers. Displays absolute value (no negatives)
void showNumber(float value)
{
  int number = abs(value); //Remove negative signs and any decimals

  //Serial.print("number: ");
  //Serial.println(number);

  for (byte x = 0 ; x < 2 ; x++)
  {
    int remainder = number % 10;

    postNumber(remainder, false);

    number /= 10;
  }

  //Latch the current segment data
  digitalWrite(segmentLatch, LOW);
  digitalWrite(segmentLatch, HIGH); //Register moves storage register on the rising edge of RCK
}

//Given a number, or '-', shifts it out to the display
void postNumber(byte number, boolean decimal)
{
  //    -  A
  //   / / F/B
  //    -  G
  //   / / E/C
  //    -. D/DP

#define a  1<<0
#define b  1<<6
#define c  1<<5
#define d  1<<4
#define e  1<<3
#define f  1<<1
#define g  1<<2
#define dp 1<<7

  byte segments;

  switch (number)
  {
    case 1: segments = b | c; break;
    case 2: segments = a | b | d | e | g; break;
    case 3: segments = a | b | c | d | g; break;
    case 4: segments = f | g | b | c; break;
    case 5: segments = a | f | g | c | d; break;
    case 6: segments = a | f | g | e | c | d; break;
    case 7: segments = a | b | c; break;
    case 8: segments = a | b | c | d | e | f | g; break;
    case 9: segments = a | b | c | d | f | g; break;
    case 0: segments = a | b | c | d | e | f; break;
    case ' ': segments = 0; break;
    case 'c': segments = g | e | d; break;
    case '-': segments = g; break;
  }

  if (decimal) segments |= dp;

  //Clock these bits out to the drivers
  for (byte x = 0 ; x < 8 ; x++)
  {
    digitalWrite(segmentClock, LOW);
    digitalWrite(segmentData, segments & 1 << (7 - x));
    digitalWrite(segmentClock, HIGH); //Data transfers to the register on the rising edge of SRCK
  }
}

Run

Upload the sketch to your Arduino, and plug the 12V adapter into the Arduino.

Provide 12V to the Arduino to power the large 7 segment display

Flip the 7-segment display over. You should see it count the digits 0-9 (the decimal point will appear on 9).

Single digit powered by HX711