Comments: IR Control Kit Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #1634254 / about 6 years ago * / 1

    The IRremote library (as of version 2.5.0) renamed several variables. The SparkFun program breaks when trying to compile with versions newer than 2.2.3. The applicable name changes are:
    RAWBUF --> RAW_BUFFER_LENGTH
    USECPERTICK --> MICROS_PER_TICK
    MARK_EXCESS --> MARK_EXCESS_MICROS

    I hope this helps someone else who is trying to use this program with newer versions of IRremote.

  • Member #1371583 / about 9 years ago / 1

    Anybody please tell me the format of the output generated by the remote . is it NEC or just a 32 bit data. I try to interface with XBee but it is not working because TSOP38238 IR receiver module is decoding the input from the remote . It is not understandable by XBee for serial read. Then I used MCP2120 to convert to UART but I want to know the format of remote so that I can able to decode the data.

  • -------------------- Tech Support Tips/Troubleshooting/Common Issues --------------------

    Additional IR Tutorials

    "Laser" Limbo [ https://www.sparkfun.com/tutorials/327 ]

  • Member #619848 / about 12 years ago / 1

    I've used the examples to set up the IR receiver on one UNO and the IR transmitter on another UNO. I can get the receiver to recognize the output of the transmitter as long as they are about 6 inches apart or less. How do I get the type of range of transmission that the remote gives me? I need across-the-room type of range -- like 15 feet or so. Thanks in advance for helping out!

  • Parizival / about 13 years ago / 1

    I can get the sketches to compile on my Uno, but I cant get them to compile on my Leonardo. Does anybody know why?

  • Member #533144 / about 13 years ago / 1

    Hello

    I saw your good site Can you help me to decode an remote IR signal ?

    Here is what i did :

    1. Increase the Rawbuf to 250 because my signal seems to be more longer than 100.

    2. Load the IRremote: IRrecvDump sketch

    3. Capture the signal (below)

    50A4250F Unknown encoding: 50A4250F (32 bits) Raw (250): -23928 3400 -1700 500 -1200 450 -1250 450 -400 450 -400 550 -350 500 -1200 500 -350 450 -400 450 -1250 450 -1300 400 -450 500 -1200 450 -400 450 -400 550 -1200 500 -1200 450 -400 450 -1250 450 -1250 450 -400 450 -450 400 -1300 450 -400 450 -400 450 -1250 500 -350 450 -450 500 -350 450 -400 450 -400 500 -350 500 -400 450 -400 400 -450 500 -350 500 -350 500 -350 500 -400 450 -400 500 -350 500 -350 500 -350 500 -350 500 -400 500 -350 500 -1200 450 -400 450 -400 450 -450 400 -450 500 -350 500 -1200 500 -350 450 -400 550 -350 500 -350 500 -350 500 -1200 500 -350 500 -400 450 -400 500 -350 500 -350 500 -350 500 -400 450 -400 450 -400 500 -350 500 -1200 500 -1200 450 -400 450 -400 500 -1250 450 -400 450 -1250 500 -350 550 -350 400 -450 500 -1200 450 -400 500 -1200 450 -1250 450 -1250 550 -350 400 -1300 450 -1250 450 -1250 500 -350 450 -400 450 -450 450 -400 500 -350 500 -350 500 -350 500 -350 450 -450 500 -350 450 -400 500 -350 500 -350 550 -300 550 -350 450 -400 500 -350 500 -350 500 -350 500 -400 450 -400 500 -350 500 -350 500 -350 500 -350 500 -350 500 -400 450 -400 450 -400 500 -350 500 -350 500 -350 500 -400 400 -450 500 -350 500 -350 450

    1. Remove the first -23928 and all the -

    2. Build and load this code

    include <IRremote.h>

    IRsend irsend;

    // setup my arrays for each signal I want to send unsigned int powerOn[250] = { 3400,1700,450,1250,450,1250,450,400,450,400,450,450,500,1200,500,350,450,400,500,1200,450,1250,550,350,500,1200,500,350,450,400,500,1200,450,1250,450,450,500,1200,450,1250,450,400,500,350,450,1300,400,450,500,350,500,1200,450,400,500,350,500,400,450,400,500,350,500,350,500,350,500,350,500,400,500,350,500,350,500,350,500,350,500,350,550,350,450,400,500,350,500,350,500,400,450,400,500,1200,500,350,500,350,500,350,550,350,450,400,500,1200,450,400,500,350,500,350,500,400,500,350,500,1200,500,350,500,350,500,350,500,350,500,400,500,350,500,350,500,350,500,350,500,350,500,1250,500,1200,400,450,500,350,500,1200,450,400,500,1200,550,350,450,400,500,350,500,1200,500,350,500,350,500,1250,450,1250,400,450,500,1200,450,1250,450,1250,450,450,450,400,450,400,500,350,500,350,500,350,550,350,450,400,450,400,500,350,500,350,500,350,500,400,500,350,500,350,500,350,500,350,500,400,450,400,500,350,500,350,450,400,500,350,550,350,450,400,500,350,450,400,450,400,500,350,550,350,500,350,450,400,500,350,500,350,500,350,500,350,500};

    void setup() { }

    void loop() { irsend.sendRaw(powerOn,250,38); delay(4000); }

    Nothing work , can you advise ? Thanks

  • a2304 / about 13 years ago / 1

    So I had a few errors with the code. What should I do?

    IR_Control_Kit:51: error: 'IRrecv' does not name a type IR_Control_Kit:52: error: 'decode_results' does not name a type IR_Control_Kit.ino: In function 'void setup()': IR_Control_Kit:70: error: 'irrecv' was not declared in this scope IR_Control_Kit.ino: In function 'void loop()': IR_Control_Kit:84: error: 'irrecv' was not declared in this scope IR_Control_Kit:84: error: 'results' was not declared in this scope


If you've found an issue with this tutorial content, please send us your feedback!