Importing Custom Images into Eagle

≡ Pages
Contributors: Shawn Hymel

Method 2: Import DXF

AutoCAD developed the Data Exchange Format (.DXF) to allow for sharing of files between AutoCAD and other programs. Lucky for us, newer versions of Eagle (7.7.0+) can also import DXF files. We can use that to add custom artwork to a layer.

Note: We'll be using Inkscape to prepare the DXF for importing. Also, note that this method results in an outline of the shape, not a complete fill.

Download Inkscape

If you don't already have it, download and install the latest version of Inkscape. You will need it for this method.

Draw or Import Image

Draw, download, import, etc. your desired image. Make sure it is a single color (we'll use black) and saved as a vector graphic (e.g. SVG). In this example, we'll import an image made with Adobe Illustrator and saved as an SVG.

Note: If your original image is a bitmap, you can also use Inkscape's bitmap tracing tool to make a vector graphic.

Change Image to Standard Size

Click the select tool (F1), and select Edit > Select All in All Layers (Ctrl + Alt + a).

alt text

Click the button to lock the height/width ratio.

alt text

Change the units to mm, and change height to 100.

alt text

Go to File > Document Properties..., select Resize page to content... drop down, and click Resize page to drawing or selection.

alt text

Massage Nodes

Convert the object to a path and select nodes:

  • Path > Object to Path (Shift + Ctrl + c)
  • Object > Ungroup (Shift + Ctrl + g) - Press this a number of times to make sure all objects have been ungrouped
  • Select all nodes with the path editor tool (F2, Ctrl + a)

alt text

Add interpolated nodes and flatten beziers (we want straight lines for the polygon):

  • Extensions > Modify Path > Add Nodes - Leave defaults, click Apply, and close the pop-up window
  • Select the nodes again (F2, Ctrl + a)
  • Extensions > Modify Path > Flatten Beziers - Leave defaults, click Apply, and close the pop-up window

alt text

Cut Closed Loops

Any shapes that have a closed loop or a "hole," you'll need to cut them (Eagle doesn't know how to create a polygon with a hole in it).

Draw a shape, such as a rectangle, that divides the hole.

alt text

Hold Shift, and select both the rectangle and your image. Select Path > Division (Ctrl + /). Repeat this process for any closed loops in your image, such as donuts, outlines, and letters like 'o' and 'd'. You should end up with a number of paths that make up your image.

alt text

Select all nodes with the path editor tool (F2, Ctrl + a). Click Path > Break Apart (Shift + Ctrl + k).

alt text

Export as DXF

Click File > Save As, give your file a name (make sure to include the .dxf extension!), and select Desktop Cutting Plotter (R13) (*.dxf) from the Save as type: drop-down menu. Click Save.

alt text

Make sure use LWPOLYLINE type of output is selected, and click OK.

alt text

Import DXF in Eagle

Start Eagle, and either create a new footprint or open your layout where you want to import the graphic.

Enter the command

run import-dxf

Click Browse to select your DXF file. Select the target layer, and change the scale as desired.

alt text

Click OK and Run on the pop-up window to import the image. Because the outline is made of lines, you can delete, move, and add lines as needed.

alt text