ESP8266 Powered Propane Poofer

≡ Pages
Contributors: Nick Poole

Programming the Thing

The firmware that we're using for the Thing board is based on the AP Web Server example code. This example code sets the Thing board up as a wireless access-point and serves a simple webpage to any connected client. Most of the magic is in the ESP8266WiFi library, so the sketch itself isn't very long at all. Let's take a look at it:

language:c

#include <ESP8266WiFi.h>

//////////////////////
// WiFi Definitions //
//////////////////////
const char WiFiAPPSK[] = "sparkfun";

/////////////////////
// Pin Definitions //
/////////////////////
const int VENT1_PIN = 4; // 
const int VENT2_PIN = 0; // 
const int IGNITION_PIN = 13; // 

WiFiServer server(80);

void setup() 
{
  initHardware();
  setupWiFi();
  server.begin();
}

void loop() 
{
  // Check if a client has connected
  WiFiClient client = server.available();
  if (!client) {
    return;
  }

  // Read the first line of the request
  String req = client.readStringUntil('\r');
  Serial.println(req);
  client.flush();

  // Match the request
  int val = -1;
  if (req.indexOf("/vent1/1") != -1)
    val = 0; 
  else if (req.indexOf("/vent2/1") != -1)
    val = 2; 
  else if (req.indexOf("/vent_all/1") != -1)
    val = 3;
  else if (req.indexOf("/ignition/1") != -1)
    val = 4; 
  else if (req.indexOf("/ignition/0") != -1)
    val = 5;

  // Set GPIO according to the request

  if (val == 0){
    digitalWrite(VENT1_PIN, 1);
    delay(500);
    digitalWrite(VENT1_PIN, 0);}

  else if (val == 2){
    digitalWrite(VENT2_PIN, 1);
    delay(500);
    digitalWrite(VENT2_PIN, 0);}

  else if (val == 3){
    digitalWrite(VENT1_PIN, 1);
    digitalWrite(VENT2_PIN, 1);
    delay(500);
    digitalWrite(VENT1_PIN, 0);
    digitalWrite(VENT2_PIN, 0);}

  else if (val == 4){
    digitalWrite(IGNITION_PIN, 1);}

  else if (val == 5){
    digitalWrite(IGNITION_PIN, 0);}

  client.flush();

  // Prepare the response. Start with the common header:
  String s = "HTTP/1.1 200 OK\r\n";
  s += "Content-Type: text/html\r\n\r\n";
  s += "<!DOCTYPE HTML>\r\n<html>\r\n";

  if ( digitalRead(IGNITION_PIN) == 0 ){
  s += "Ignitior is currently turned OFF.";}
  else{
  s += "Ignitior is currently turned ON.";}
  s += "<br><br>\r\n"; // Go to the next line.

  s += "<a href = \"/ignition/1\">Glow Ingition On</a><br>\r\n";
  s += "<a href = \"/ignition/0\">Glow Ingition Off</a><br>\r\n";
  s += "<a href = \"/vent1/1\">Vent Tank 1 (500ms)</a><br>\r\n";
  s += "<a href = \"/vent2/1\">Vent Tank 2 (500ms)</a><br>\r\n";
  s += "<a href = \"/vent_all/1\">Vent Both Tanks (500ms)</a><br>\r\n";

  s += "</html>\n";

  // Send the response to the client
  client.print(s);
  delay(1);
  Serial.println("Client disonnected");

  // The client will actually be disconnected 
  // when the function returns and 'client' object is detroyed
}

void setupWiFi()
{
  WiFi.mode(WIFI_AP);

  // Do a little work to get a unique-ish name. Append the
  // last two bytes of the MAC (HEX'd) to "Thing-":
  uint8_t mac[WL_MAC_ADDR_LENGTH];
  WiFi.softAPmacAddress(mac);
  String macID = String(mac[WL_MAC_ADDR_LENGTH - 2], HEX) +
                 String(mac[WL_MAC_ADDR_LENGTH - 1], HEX);
  macID.toUpperCase();
  String AP_NameString = "ESP8266 Flame Cannon " + macID;

  char AP_NameChar[AP_NameString.length() + 1];
  memset(AP_NameChar, 0, AP_NameString.length() + 1);

  for (int i=0; i<AP_NameString.length(); i++)
    AP_NameChar[i] = AP_NameString.charAt(i);

  WiFi.softAP(AP_NameChar, WiFiAPPSK);
}

void initHardware()
{
  Serial.begin(115200);
  pinMode(VENT1_PIN, OUTPUT);
  digitalWrite(VENT1_PIN, LOW);
  pinMode(VENT2_PIN, OUTPUT);
  digitalWrite(VENT2_PIN, LOW);
  pinMode(IGNITION_PIN, OUTPUT);
  digitalWrite(IGNITION_PIN, LOW);

}

Because this code is essentially an expanded version of the example code, I won't dive into it too deeply here. That being said, let's look at what's changed:

Matching Requests

While the example code was only looking for 3 possible valid requests, we'll be looking for any of 5: Ignition On, Ignition Off, Vent Tank 1, Vent Tank 2 and Vent All. We handle these requests by assigning a value to each like this:

language:c
  if (req.indexOf("/vent1/1") != -1)
    val = 0; 
  else if (req.indexOf("/vent2/1") != -1)
    val = 2; 
  else if (req.indexOf("/vent_all/1") != -1)
    val = 3;
  else if (req.indexOf("/ignition/1") != -1)
    val = 4; 
  else if (req.indexOf("/ignition/0") != -1)
    val = 5;

When we send our response, we'll include hyperlinks for each of these requests.

Setting the GPIO

language:c
 if (val == 0){ // Vent Tank 1
    digitalWrite(VENT1_PIN, 1);
    delay(500);
    digitalWrite(VENT1_PIN, 0);}

  else if (val == 2){ // Vent Tank 2
    digitalWrite(VENT2_PIN, 1);
    delay(500);
    digitalWrite(VENT2_PIN, 0);}

  else if (val == 3){ // Vent All
    digitalWrite(VENT1_PIN, 1);
    digitalWrite(VENT2_PIN, 1);
    delay(500);
    digitalWrite(VENT1_PIN, 0);
    digitalWrite(VENT2_PIN, 0);}

  else if (val == 4){ // Ignition On
    digitalWrite(IGNITION_PIN, 1);}

  else if (val == 5){ // Ignition Off
    digitalWrite(IGNITION_PIN, 0);}

Each valid request has an associated GPIO call to open or close a relay. The "Vent Tank" requests simply close the relay for half a second, and then release it. Requests made to the ignitor set it to either the on or off position until further notice.

Formulating a Reply

Our server's reply will always be a list of hyperlinks that make it easy to quickly fire valid requests. At the top of the list, we'll add an indicator to let us know whether we have the ignitor turned on. Each line of the html response is appended to a string object and sent to the server library to be relayed to the client. The html reponse, without the weird formatting, looks like this:

  HTTP/1.1 200 OK
  Content-Type: text/html
  <!DOCTYPE HTML>

  <html>

  Ignitior is currently turned ON.<br>
  <a href = "/ignition/1">Glow Ingition On</a><br>
  <a href = "/ignition/0">Glow Ingition Off</a><br>
  <a href = "/vent1/1">Vent Tank 1 (500ms)</a><br>
  <a href = "/vent2/1">Vent Tank 2 (500ms)</a><br>
  <a href = "/vent_all/1">Vent Both Tanks (500ms)</a><br>

  </html>