CryptoCape Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: jbdatko, CaseyTheRobot

Cape EEPROM

alt text

The Cape's EEPROM is defaulted to an I2C address of 0x57. If you plan on stacking capes -- the BeagleBone can support up to four stacked capes -- you may need to change the addresses of the EEPROM. The table below contains the available addresses for the EEPROM. Close the appropriate jumpers to change the address. (0 - Closed, 1 - Open).

Address Table

A2 A1 A0 7-bit address
1 0 0
0x54
1 0 1
0x55
1 1 0
0x56
1 1 1
0x57

If you want to prevent users from writing to the EEPROM, you'll need to solder 0.1" male headers to the write protect pads and place a jumper on these pins. The EEPROM contains the cape definition, which is written during manufacturing and testing. If you overwrite it, the cape may not load correctly. You can always read the EEPROM with the following command:

sudo cat /sys/bus/i2c/devices/1-0057/eeprom| hexdump -C