CP2102 USB to Serial Converter Hook-Up Guide

≡ Pages
Contributors: Toni_K

Overview

The CP2102 Breakout Board is a great tool for embedded systems that require a serial connection to a computer. The board attaches to the USB bus via a standard type B female connector, and appears as a standard COM port.

CP2102 Breakout Board

This IC doesn't require any external oscillator, has an on-board voltage regulator, and uses reprogrammable internal EEPROM for the device description. The full hardware UART has flow control for baud rates from 300bps to 921600bps. This breakout also allows you to connect the TX/RX pins of your favorite microcontroller or serial application to the RX/TX pins of the breakout, creating a simple serial cable replacement.

Required Materials

You will need the following materials to complete this hookup guide.

You will also need standard soldering tools to complete the circuit.

Suggested Reading

If you are not comfortable with the following concepts, you should review them before moving ahead with the CP2102 breaout board.