CCS811 Air Quality Breakout Hookup Guide
Contributors:
MTaylor
Resources and Going Further
Now that you've successfully got your CCS811 breakout up and running, and have scientifically proved which family member is the smelliest, here are some additional resources:
- CCS811 Datasheet-DS000459.pdf --- PDF
- ASHRAE Allowable CO2 Levels.pdf --- PDF
- CC-000774-AN-3-Assembly guidelines for CCS811.pdf --- PDF
- CC-000783-AN-1-Mechanical Considerations for CCS811_0.pdf --- PDF
- CCS811 Firmware Download AN000371.pdf --- PDF
- CCS811 Programming Guide-AN000369.pdf --- PDF
- CCS811 Thermistor Interface AN000372.pdf --- PDF
- Indoor Air Quality Investigations TVOCs EU.pdf --- PDF
- CCS811_Air_Quality_Breakout product repository --- Design files and docs
- SparkFun_CCS811_Arduino_Library Repository --- Source and example files for the Arduino library used in this tutorial.
Also, the following examples are included with the library but not discussed. They may help you on your way!
- BaselineOperator --- Save and restore baselines to the EEPROM
- Core --- Show how the underlying hardware object works
- TwentyMinuteTest --- Report data with timestamp
Need some inspiration for your next project? Check out some of these sensor-related tutorials:
Getting Started with Load Cells
A tutorial defining what a load cell is and how to use one.
ESP32 Thing Motion Shield Hookup Guide
Getting started with the ESP32 Thing Motion Shield to detect movements using the on-board LSM9DS1 IMU and adding a GPS receiver. Data can be easily logged by adding an microSD card to the slot.
Getting Started with the A111 Pulsed Radar Sensor
Get started with the Acconeer A111 SDK with a Raspberry Pi! The tiny A111 pulsed coherent radar (PCR) adds high-precision, cutting-edge distance measurement for speed-, material-, motion-, or gesture-sensing projects! We’re not talking about simple ultrasonic, or even infrared sensors here, but 60GHz radar!
Air Velocity Sensor Breakout - FS3000 Hookup Guide
Get started with the Air Velocity Sensor Breakout - FS3000!
Or maybe check out our tests using the sensor at SparkFun!