APA102 Addressable LED Hookup Guide

≡ Pages
Contributors: bboyho

Resources and Going Further

Accessories

Try writing some additional code and adding more features in order to change the brightness or mode with the APA102 using a potentiometer or button. Or try adding a sensor to trigger animations based on sound to react to the beat of a track!

Trimpot 10K Ohm with Knob

COM-09806
$1.25

SparkFun Sound Detector (with Headers)

SEN-14262
$13.95

Multicolor Buttons - 4-pack

PRT-14460
$1.95

SparkFun Capacitive Touch Slider - CAP1203 (Qwiic)

SEN-15344
$7.95

Depending on the design, there are some shields for the Teensy that breakout pins for the APA102. Just make sure to check the wiring to ensure that it matches the connection for the LED strips.

Teensy Prop Shield LC

DEV-13996
Retired

For more information about the APA102, check out the resources below:

Now that you've got the gist of the APA102's, how are you going to use it in a project? Need some inspiration? Check out these tutorials for ideas to diffuse or daisy chain longer strips:

Building Large LED Installations

Learn what it takes to build large LED installations from planning to power requirements to execution.

LED Cloud-Connected Cloud

Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!

Mean Well LED Switching Power Supply Hookup Guide

In this tutorial, we will be connecting a Mean Well LED switching power supply to an addressable LED strip controlled by an Arduino.

SparkFun ESP32 DMX to LED Shield

Learn how to utilize your DMX to LED Shield in a variety of different ways.

Or check out some of these blog posts for ideas:

LEDs