APA102 Addressable LED Hookup Guide

≡ Pages
Contributors: bboyho

LuMini

The LuMini is a miniaturized version of the Lumenati LEDs. The LuMini uses the APA102-2020 size for tight pixel densities. While they have a higher resolution, the tradeoff is there is a limitation in how bright they can be turned on. Having a high brightness can result in damage to the LED and PCB due the ability to dissipate heat with the small package.

LuMini Ring - 2 Inch Version LuMini Matrix
LuMini Ring - 2 Inch Version LuMini Matrix

For more information, check out the following tutorials to get started.

LuMini Ring Hookup Guide

January 17, 2019
The LuMini Rings (APA102-2020) are the highest resolution LED rings available.

LuMini 8x8 Matrix Hookup Guide

January 24, 2019
The LuMini 8x8 Matrix (APA102-2020) are the highest resolution LED matrix available.