ACS712 Low Current Sensor Hookup Guide

This Tutorial is Retired!

Note: This tutorial is for the ACS712 Current Sensor Breakout Boards. If you are using either of the newer ACS723 Breakout Boards, please refer to the new Current Sensor Breakout (ACS723) Hookup Guide.

View the updated tutorial: Current Sensor Breakout (ACS723) Hookup Guide

≡ Pages
Contributors: AGlass0fMilk

Resources and Going Further

The ACS712 sensor is ideal if you need to measure a small to moderate amount of current, especially if it's AC current! For more information about the ACS712, check out the links below:

If you don't need electrical isolation and want to measure smaller currents, check out the INA169 Breakout Board. And for even higher power applications, check out the Non-Invasive Current Sensor - 30A.

Non-Invasive Current Sensor - 30A

SEN-11005
$14.95

SparkFun Current Sensor Breakout - INA169

SEN-12040
$13.93

For more power related learning, check out the tutorials below:

Beefcake Relay Control Hookup Guide

This is a guide for assembling and basic use of the Beefcake Relay Control board

Internet of Things Experiment Guide

The SparkFun ESP8266 Thing Dev Board is a powerful development platform that lets you connect your hardware projects to the Internet. In this guide, we show you how to combine some simple components to remotely log temperature data, send yourself texts and control lights from afar.

SparkFun 5V/1A LiPo Charger/Booster Hookup Guide

This tutorial shows you how to hook up and use the SparkFun 5V/1A LiPo Charger/Booster circuit.

Hookup Guide for the SparkFun RedBoard Artemis ATP

Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module wrapped in the Mega Arduino Footprint