ACS712 Low Current Sensor Hookup Guide

This Tutorial is Retired!

Note: This tutorial is for the ACS712 Current Sensor Breakout Boards. If you are using either of the newer ACS723 Breakout Boards, please refer to the new Current Sensor Breakout (ACS723) Hookup Guide.

View the updated tutorial: Current Sensor Breakout (ACS723) Hookup Guide

≡ Pages
Contributors: AGlass0fMilk

Introduction

The ACS712 is a handy little current sensor from Allegro MicroSystems for low to moderate current sensing applications. SparkFun offers two flavors of breakout board, one with just the sensor and another with an on-board amplifier to increase the sensitivity.

SparkFun Hall-Effect Current Sensor Breakout - ACS712

BOB-08882
Retired

SparkFun Low Current Sensor Breakout - ACS712

SEN-08883
Retired

The ACS712 sensor uses a Hall effect sensor to output a voltage relative to the current flowing through the IP+ and IP- pins. The advantage of using a Hall effect sensor is that the circuit being sensed and the circuit reading the sensor are electrically isolated. This means that, although your Arduino is running on 5V, the sensed circuit can be operating at higher DC or AC voltages!

The amplified breakout board is capable of sensing very small currents down to around 10mA and large currents up to 5A! However, since the output is analog, your usable readings will be limited by noise and the resolution of the ADC reading the output. This sensor is not recommended for current sensing lower than 10's of milliamps.

Required Materials

Depending on the equipment available to you, you will need some of the following items to follow along with this hookup guide:

Suggested Reading

Here are some topics related to this hookup guide you may want to review: